System clock configuring with stm32cube
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-01-02 2:44 AM
Posted on January 02, 2015 at 11:44
Hello
I have 2 questions :1 - According to this library and sample examples , HAL_Init() function is called at the start of the main() that configures the systemtick timer for generating 1ms interrupts , but after that the SystemClock_Config() is called which configures the plls and other clock related parameters for increasing core clock to 168 MHz(for example for stm32f4) .But by this work , the systick timer will not make precesion interrupts anymore because its time base has changed without any updating .2 - According to page 368 of RM0090 , SysTick has fixed calibration value with HCLK set to 150 MHz but we have 168 MHz in stm32f4 , So its time base is not 1 ms and can not be changed, is it right ?Please help, thanks .
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-02-28 9:26 AM
Posted on February 28, 2015 at 18:26Anyone to answer?