cancel
Showing results for 
Search instead for 
Did you mean: 

SWO doesn't show up in ST-Link

Josh Yu
Associate II

Posted on February 06, 2017 at 17:58

I'm really stumped on this one. I have a STM32F411 chip on a Wifi module and I'm trying to get the Serial Wire Output to work. My configuration code is below. Now I can see that there's some signal on the SWO line under the oscilloscope. The signal is about 3.1V peak to peak, but biased around 0V (i.e. signal is changing between -1.5V to 1.5V). On my computer, ST-Link Utility shows nothing in the Serial Wire Viewer. My clock is configured to be 96MHz through PLL and the ST-Link automatically chooses 2MHz for the SWO frequency. However, the signal from the oscilloscope looks more like 1MHz. Any idea on how I can fix this?

/* Configure Trace Port Interface Unit */

   CoreDebug->DEMCR |= CoreDebug_DEMCR_TRCENA_Msk; // Enable access to registers

   TPI->ACPR = 47; // Trace clock = HCLK/(x+1) = 2MHz

   TPI->SPPR = 2; // Pin protocol = NRZ/USART

   TPI->FFCR = 0x102; // TPIU packet framing enabled when bit 2 is set.

                 // You can use 0x100 if you only need DWT/ITM and not ETM.

   /* Configure PC sampling and exception trace */

   DWT->CTRL = (1 << DWT_CTRL_CYCTAP_Pos) // Prescaler for PC sampling

                                // 0 = x32, 1 = x512

          | (0 << DWT_CTRL_POSTPRESET_Pos) // Postscaler for PC sampling

                                    // Divider = value + 1

          | (1 << DWT_CTRL_PCSAMPLENA_Pos) // Enable PC sampling

          | (2 << DWT_CTRL_SYNCTAP_Pos)   // Sync packet interval

                                   // 0 = Off, 1 = Every 2^23 cycles,

                                   // 2 = Every 2^25, 3 = Every 2^27

          | (1 << DWT_CTRL_EXCTRCENA_Pos) // Enable exception trace

          | (1 << DWT_CTRL_CYCCNTENA_Pos); // Enable cycle counter

   DBGMCU->CR = DBGMCU_CR_TRACE_IOEN; // Enable IO trace pins

   /* Configure instrumentation trace macroblock */

   ITM->LAR = 0xC5ACCE55;

   ITM->TCR = (1 << ITM_TCR_TraceBusID_Pos) // Trace bus ID for TPIU

         | (1 << ITM_TCR_DWTENA_Pos) // Enable events from DWT

         | (1 << ITM_TCR_SYNCENA_Pos) // Enable sync packets

         | (1 << ITM_TCR_ITMENA_Pos); // Main enable for ITM

   ITM->TPR = 0xF;

   ITM->TER = 0xFFFFFFFF; // Enable all stimulus ports

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Josh Yu
Associate II
Posted on February 06, 2017 at 23:57

I figured it out. As it turned out I mistakenly swapped the TDI and TDO traces on my PCB and I wasn't getting any SWO through the ST-Link because it's the wrong pin. Stupid mistakes >_<

View solution in original post

4 REPLIES 4
Oliver Beirne
Senior

Posted on February 06, 2017 at 18:57

Hi Josh

I have moved your question to the

https://community.st.com/s/topic/0TO0X000000BSqSWAW/

where someone should be able to assist you.

Thanks

Posted on February 06, 2017 at 22:21

Does the M4 even use the LAR?

What if you don't configure all this stuff? The ST-LINK Utilities should configure things based on the supplied Core MHz

How about something as minimal as this

      *((u32 *)0xE0042004) |= 0x27;

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on February 06, 2017 at 22:43

Hey Clive,

I tried both disabling the configuration and only having that one line you provided. But then the SWO line doesn't show up on the oscilloscope anymore.

In the core_cm4.h the LAR is defined. The RM0383 page 815 shows the Lock Access Register.

Thanks,

Josh

Josh Yu
Associate II
Posted on February 06, 2017 at 23:57

I figured it out. As it turned out I mistakenly swapped the TDI and TDO traces on my PCB and I wasn't getting any SWO through the ST-Link because it's the wrong pin. Stupid mistakes >_<