cancel
Showing results for 
Search instead for 
Did you mean: 

Strange behaviour with USART interrupt - STM32F3discovery

andreaspiezia9
Associate III
Posted on January 16, 2014 at 20:08

Hi all,

the following code works fine if I comment the line 131: OutString(''In full\n'');

But it doesn't give the echo character if a don't comment the line.

I don't understand why.

Your help is much appreciate.

<code>

/* Includes ------------------------------------------------------------------*/

#include ''main.h''

#include <string.h> // memcpy()

  /*!< At this stage the microcontroller clock setting is already configured, 

       this is done through SystemInit() function which is called from startup

       file (startup_stm32f30x.s) before to branch to application main.

       To reconfigure the default setting of SystemInit() function, refer to

       system_stm32f30x.c file

     */ 

  

// STM32 USART2 LOOP (Tx PA.2, Rx PA.3) STM32F3xx - sourcer32@gmail.com

 

#include ''stm32f30x.h''

volatile char StringLoop[] = ''Conta\r\n'';

volatile int full = 0;

volatile uint16_t ch;

 

/**************************************************************************************/

 

void RCC_Configuration(void)

{

  /* Enable GPIO clock */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);

 

  /* Enable USART clock */

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

}

 

/**************************************************************************************/

 

void GPIO_Configuration(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

/*-------------------------- GPIO Configuration ----------------------------*/

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOA, &GPIO_InitStructure);

/* Connect USART pins to AF */

  

/* Configure Alternate Function pin muxing fabric to escape USART2 Rx and Tx */

GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_7); //USART2_TX

GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_7); //USART2_RX

}

 

/**************************************************************************************/

 

void USART2_Configuration(void)

{

USART_InitTypeDef USART_InitStructure;

/* USARTx configuration ------------------------------------------------------*/

/* USARTx configured as follow:

        - BaudRate = 4800 baud

        - Word Length = 8 Bits

        - One Stop Bit

        - No parity

        - Hardware flow control disabled (RTS and CTS signals)

        - Receive and transmit enabled

  */

USART_InitStructure.USART_BaudRate = 4800;

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

USART_Init(USART2, &USART_InitStructure);

USART_Cmd(USART2, ENABLE);

USART_ITConfig(USART2, USART_IT_RXNE, ENABLE); // Enable USART2 Receive Interrupt

}

 

/**************************************************************************************/

  

void NVIC_Configuration(void)

{

  NVIC_InitTypeDef NVIC_InitStructure;

  

  /* Configure the NVIC Preemption Priority Bits */

  NVIC_PriorityGroupConfig(NVIC_PriorityGroup_0);

  

  /* Enable the USART3 Interrupt */

  NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);

}

  

/**************************************************************************************/

 void OutString(char *s)

{

    while(*s)

    {

      while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty

 

    USART_SendData(USART2, *s++);

    }

}

/**************************************************************************************/

  

void USART2_IRQHandler(void)

{

    while(USART_GetFlagStatus(USART2, USART_FLAG_RXNE) == RESET); // Wait for Char

    ch  = USART_ReceiveData(USART2); // Collect Char7

full = 1;

}

 

/**************************************************************************************/

int main(void)

{

RCC_Configuration();

  GPIO_Configuration();

  NVIC_Configuration();

  USART2_Configuration();

OutString(''This is an echo test for USART interrupt\n'');

while(1)

{

if(full)

{

OutString(''In full\n'');

while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty

USART_SendData(USART2, ch); // Echo Char

full = 0;

}

}

}

 

/**************************************************************************************/

 

#ifdef  USE_FULL_ASSERT

 

/**

  * @brief  Reports the name of the source file and the source line number

  *         where the assert_param error has occurred.

  * @param  file: pointer to the source file name

  * @param  line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{

  /* User can add his own implementation to report the file name and line number,

     ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

 

  /* Infinite loop */

  while (1)

  {

  }

}

#endif

<\code>

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
andreaspiezia9
Associate III
Posted on January 16, 2014 at 20:11

Here below the output with line uncommented:

<code>This is an echo test for USART interrupt

p //character from keyboard

In full

u //character from keyboard

In full

y //character from keyboard

In full </code>