2017-07-17 10:43 PM
Hi everyone,
I use CAN interrupt to receive CAN message, the CAN ID is 0x500 that is lower than other CAN IDs what I received.
but this CAN message can not received frequency. sometimes it will loss.
So I don't know where is wrong. could you help me?
thanks!
for My Initial code & CAN interrupt code is below:
u8 CAN_Mode_Init(u8 tsjw,u8 tbs2,u8 tbs1,u16 brp,u8 mode)
{ CAN_InitTypeDef CAN_InitStructure; CAN_FilterInitTypeDef CAN_FilterInitStructure; /*init can */ CAN_InitStructure.CAN_TTCM=DISABLE; CAN_InitStructure.CAN_ABOM=ENABLE; CAN_InitStructure.CAN_AWUM=DISABLE; CAN_InitStructure.CAN_NART=DISABLE; CAN_InitStructure.CAN_RFLM=DISABLE; CAN_InitStructure.CAN_TXFP=DISABLE; CAN_InitStructure.CAN_Mode= mode; /*set baud rate*/ CAN_InitStructure.CAN_SJW=tsjw; CAN_InitStructure.CAN_BS1=tbs1; CAN_InitStructure.CAN_BS2=tbs2; CAN_InitStructure.CAN_Prescaler=brp; CAN_Init(CAN1, &CAN_InitStructure); /*init filter/mask*/ CAN_FilterInitStructure.CAN_FilterNumber=0; //filter 0 CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdList; //mask mode CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_16bit; //filter scale /*id list is id1 id2 id3 id4*/ CAN_FilterInitStructure.CAN_FilterIdHigh=VCU_HMI_ID1<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterIdLow=VCU_HMI_ID2<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterMaskIdHigh=VCU_HMI_ID3<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterMaskIdLow=VCU_HMI_ID4<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterFIFOAssignment=CAN_Filter_FIFO0; CAN_FilterInitStructure.CAN_FilterActivation=ENABLE; CAN_FilterInit(&CAN_FilterInitStructure); /*id list is id5 id6 id7 */ CAN_FilterInitStructure.CAN_FilterNumber=1; //filter 1 CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdList; //mask mode CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_16bit; //filter scale CAN_FilterInitStructure.CAN_FilterIdHigh=VCU_HMI_ID5<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterIdLow=VCU_HMI_ID6<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterMaskIdHigh=VCU_HMI_ID7<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterMaskIdLow=VCU_HMI_DIAGNOSE<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterFIFOAssignment=CAN_Filter_FIFO0; CAN_FilterInit(&CAN_FilterInitStructure);CAN_FilterInitStructure.CAN_FilterNumber=2; //filter 2
CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdList; //mask mode CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_16bit; //filter scale CAN_FilterInitStructure.CAN_FilterIdHigh=ABS_INFO<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterIdLow=VCU_HMI_ID8<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterMaskIdHigh=UDS_TESTER_ID<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterMaskIdLow=UDS_VCU_ID<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterFIFOAssignment=CAN_Filter_FIFO0; CAN_FilterInit(&CAN_FilterInitStructure);CAN_FilterInitStructure.CAN_FilterNumber=3; //filter 3
CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdList; //mask mode CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_16bit; //filter scale CAN_FilterInitStructure.CAN_FilterIdHigh=NETWORK_STATE<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterIdLow=BMS_VCU_07<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterMaskIdHigh=ENCRYPTION_VCU_HMI<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterMaskIdLow=NULL<<FILTER_MASK_STDID_SHIFT; CAN_FilterInitStructure.CAN_FilterFIFOAssignment=CAN_Filter_FIFO0;CAN_FilterInit(&CAN_FilterInitStructure);
return 0;}/*************************************************
Function: CanIsrRx0_0Description: recv intterruptCalled By: N AInput: recv messageOutput: can data & can idReturn: NAOthers: NA*************************************************/void CanIsrRx0_0(void){ CanRxMsg rxMessage; if(CAN_GetITStatus(CAN1,CAN_IT_FF0))//fifo full { CAN_ClearITPendingBit(CAN1,CAN_IT_FF0);//clear fifo full } else if(CAN_GetITStatus(CAN1,CAN_IT_FOV0))//overflow flag { CAN_ClearITPendingBit(CAN1,CAN_IT_FOV0);//clear overflow } else { CAN_Receive(CAN1,CAN_FIFO0, &rxMessage); CAN_ClearITPendingBit(CAN1,CAN_IT_FMP0); CAN_FIFORelease(CAN1,CAN_FIFO0); /*rx process*/ CanMessageSendRxQueue(&rxMessage); } }2017-07-18 6:39 AM
You mention 'sometimes it will loss'. What do the CAN_RF0R - FOVR0 bits tell you?