cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4xx HAL_CAN_Transmit_IT() enables interrupt before transmission

dmeise
Associate II
Posted on July 13, 2016 at 14:31

Hello,

the HAL function HAL_CAN_Transmit_IT() enables the Transmit mailbox empty Interrupt before the requesting transmission.

At least if I run the CAN bus wit 1Mbit the mailbox empty interrupt is triggered before the new frame is send.

I read abaut this problem in this forum before but also new HAL drivers are delivered with the same bug!

#can-interrupt-transmission
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
slimen
Senior
Posted on July 13, 2016 at 15:53

Hi,

It is a known bug which is confirmed by ST team, but the fix has not yet been released.

Regards

slimen
Senior
Posted on July 14, 2016 at 17:23

Hi,

Please explain with more details your problem, maybe is not the same issue that I have a look in this forum.

It's possible to share discussions which contains this problem?

Regards