2025-04-12 1:16 PM
Use SPI with MCU above. With
spi_transmit(0x55);and
void spi_transmit(uint8_t tx_data)
{
SPI1->DR= tx_data;
while (!(SPI1->SR & SPI_SR_TXE));
}I have 16 SPI clocks. Init was:
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;Data on MOSI showing on the first 8 clocks, MOSI on remaining 8 clocks is zero.
While using HAL (same init):
pdat= 0x55;
HAL_SPI_Transmit(&hspi1, (const uint8_t *)&pdat, 1, 100);I have, as expected, 8 SPI clocks.
Any Suggestions? Thanks!
Solved! Go to Solution.
2025-04-12 5:12 PM
Write 8 bits to DR instead of 16.
*(volatile uint8_t*)&SPI1->DR = tx_data;
2025-04-12 5:12 PM
Write 8 bits to DR instead of 16.
*(volatile uint8_t*)&SPI1->DR = tx_data;
2025-04-13 1:02 AM
Wow, that worked! I'm still confused, because "tx_data" is 8bits, init was for 8bit data and the subroutine already worked at an STM32F103C8T6. But it is like it is, Thanks again!
2025-04-13 6:45 AM
The access size is dictated by the left hand side of the expression and since SPI->DR is a 16-bit register, that's what you write regardless of what is on the right, which gets converted to the right size.
F103 doesn't have data packing so it works there.