cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L433 PWM on TIM16

Rogers.Gary
Senior II

Hello:

There is a post on this same issue titled "TIM16 PWM signal generation...". The fix here was to set the AOE bit in the BDTR register. In that thread they were using LL.

I am having a similar issue where I am unable to get the PWM output signal on PA.6. The code base was generated using CubeMX, this is the initialization code:

#define PULSE1_VALUE      (uint32_t)(7999)       /* Capture Compare 1 Value */

void MX_TIM16_Init(void)

{

 TIM_OC_InitTypeDef sConfigOC = {0};

 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};

 htim16.Instance = TIM16;

 htim16.Init.Prescaler = (uint32_t)999;

 htim16.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim16.Init.Period = 15999;

 htim16.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

 htim16.Init.RepetitionCounter = 0;

 htim16.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

 if (HAL_TIM_Base_Init(&htim16) != HAL_OK)

 {

   Error_Handler();

 }

 if (HAL_TIM_PWM_Init(&htim16) != HAL_OK)

 {

   Error_Handler();

 }

 sConfigOC.OCMode = TIM_OCMODE_PWM1;

 sConfigOC.Pulse = PULSE1_VALUE;

 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

 sConfigOC.OCNPolarity = TIM_OCNPOLARITY_HIGH;

 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

 sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;

 sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;

 if (HAL_TIM_PWM_ConfigChannel(&htim16, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)

 {

   Error_Handler();

 }

 sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;

 sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;

 sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;

 sBreakDeadTimeConfig.DeadTime = 0;

 sBreakDeadTimeConfig.BreakState = TIM_BREAK_DISABLE;

 sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_HIGH;

 sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_ENABLE;

 if (HAL_TIMEx_ConfigBreakDeadTime(&htim16, &sBreakDeadTimeConfig) != HAL_OK)

 {

   Error_Handler();

 }

 HAL_TIM_MspPostInit(&htim16);

}

The hardware is initialized here:

vovoid HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)

{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

 if(tim_baseHandle->Instance==TIM16)

 {

   /* TIM16 clock enable */

   __HAL_RCC_TIM16_CLK_ENABLE();

   /* TIM16 interrupt Init */

   HAL_NVIC_SetPriority(TIM1_UP_TIM16_IRQn, 5, 0);

   HAL_NVIC_EnableIRQ(TIM1_UP_TIM16_IRQn);

   __HAL_RCC_GPIOA_CLK_ENABLE();

   /**TIM16 GPIO Configuration   

   PA6    ------> TIM16_CH1

   */

   GPIO_InitStruct.Alternate = GPIO_AF14_TIM16;

   GPIO_InitStruct.Pin = GPIO_PIN_6;

   GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

   GPIO_InitStruct.Pull = GPIO_PULLUP;

   GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

   HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 }

}

}

Finally in main(), I call the start:

if (HAL_TIM_PWM_Start(&htim16, TIM_CHANNEL_1) != HAL_OK)

   {

       /* PWM Generation Error */

       Error_Handler();

   }   

As seen in the initialization, I have set the variable sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_ENABLE;

which should be the AOE bit as mentioned in the other post. Yet, there is still no signal from PA6.

Any suggestions?

NB:

I also tried a direct register update before enabling the PWM. Did not help.

 TIM16->BDTR |= TIM_BDTR_MOE;

 TIM16->BDTR |= TIM_BDTR_AOE;

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Rogers.Gary
Senior II

Solved. I had the interrupt enabled for the PWM on the channel. Disabled it and it works OK.

View solution in original post

4 REPLIES 4
waclawek.jan
Super User

Read and check all the relevant GPIO and TIM registers' content.

JW

Rogers.Gary
Senior II

The response I posted was not good information, I will repost again.

Rogers.Gary
Senior II

I generated the code with nothing else and PWM works. Still looking...

Rogers.Gary
Senior II

Solved. I had the interrupt enabled for the PWM on the channel. Disabled it and it works OK.