STM32L152: Connect the COMP2 output to the IO port
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-06-01 2:22 AM
Posted on June 01, 2018 at 11:22
I want to connect the COMP2 output to the external circuit.
I know the output can be redirected to the IC channel of some timers.
and I tried to use TIM2_IC4 to get the output of COMP2 but failed.
Is it possible to implement in STM32L152C8?
Because it is a low-power application, I do not want to use interrupt to achieve this.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0