cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L0X0 Series - No UART Half Transfer Flag/Bit Documented?

nobbyv77
Associate II

Unless I'm missing something, I don't see a HT flag documented in the STM32L0X0 reference manual in the USART_ISR register. I see the TC, idle, etc. flags. So how is that interrupt getting triggered (because I have verified it does get triggered)?

EDIT: Also don't see it if I examine the UART SFR in the CubeIDE.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

You're confusing peripheral level functionality. The DMA controller has a HT (Half-Transfer) and TC (Transfer Complete) indication allowing for a buffer to be split in a ping-pong fashion, and defining an active and inactive portion the IRQ Handler or Callback can manage without interfering with the transfer.

In the U(S)ART context TC means Transmit Complete, that all the bits in the word have crossed the wire. TXE signals when the "buffer" is empty usually as the first bit hits the wire as the buffer is moved into the shift register to move the bits across the wire.

To keep the U(S)ART busy it's usually best to fill based on TXE to insure continuity, and provide about a byte time to service the request

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

2 REPLIES 2

You're confusing peripheral level functionality. The DMA controller has a HT (Half-Transfer) and TC (Transfer Complete) indication allowing for a buffer to be split in a ping-pong fashion, and defining an active and inactive portion the IRQ Handler or Callback can manage without interfering with the transfer.

In the U(S)ART context TC means Transmit Complete, that all the bits in the word have crossed the wire. TXE signals when the "buffer" is empty usually as the first bit hits the wire as the buffer is moved into the shift register to move the bits across the wire.

To keep the U(S)ART busy it's usually best to fill based on TXE to insure continuity, and provide about a byte time to service the request

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
nobbyv77
Associate II

Ah, of course, my mistake.