cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32L082] Powering the USB section of the chip

roland van straten
Associate III

I do not want to use the USB part of the STM32L082. According to the Ref Manual RM0376 page 140 there is no explicit mention that the VCC_USB can be tied to GND if not in use. So what would be the thing to do (and reduce the power even further): GND or 3.0-3.6V?

Please advise?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0