cancel
Showing results for 
Search instead for 
Did you mean: 

stm32l051 spi receiver interrupt

chenping2
Associate
Posted on March 02, 2015 at 05:59

when i use SPI to receiver a byte from the external ADC chip, but the SPI_SR_RXNE can't be set after the data into the SPI_DR.the initialization code below:

void MX_SPI2_Config(void)

{

  

  /* Enable the peripheral clock SPI2 */

  RCC->APB1ENR |= RCC_APB1ENR_SPI2EN;

  /* DISABLE TXE IT */

  SPI2->CR2 &= ~(SPI_CR2_TXEIE | SPI_CR2_RXNEIE | SPI_CR2_ERRIE | SPI_CR2_FRF | SPI_CR2_SSOE | SPI_CR2_TXDMAEN | SPI_CR2_RXDMAEN);

  /* MASTER MODE, SCK IDLE HIGH */  

  SPI2->CR1 |= (SPI_CR1_MSTR | SPI_CR1_CPOL); 

  

  /* NSS SOFT  */   

  SPI2->CR1 |= (SPI_CR1_SSM | SPI_CR1_SSI);

  

    /* RXNE IT */

  SPI2->CR2 |= SPI_CR2_RXNEIE; 

 

  

  /* 16 bit frame mode */

  SPI2->CR1 |= SPI_CR1_DFF;

    

  /* Enable SPI2 */   

  SPI2->CR1 |= SPI_CR1_SPE;

  /* Configure IT */

  /* Set priority for SPI2_IRQn */

  NVIC_SetPriority(SPI2_IRQn, 0); 

  

  /* Enable SPI2_IRQn */  

  NVIC_EnableIRQ(SPI2_IRQn);  

  

}

void SPI2_IRQHandler(void)

{   

 if((SPI2->SR & SPI_SR_RXNE) == SPI_SR_RXNE)

 {

   SPI2_Data = SPI2->DR;

 }

}

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0