cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L031G6 flashing problem

duybienle
Associate II
Posted on September 14, 2016 at 09:26

Hi, I need to flash my code into STM32L031G6 chip using an external debugger, but i got the following error:

ERROR: Timeout while checking target RAM, RAMCode did not respond in time

 

Failed to prepare for programming.

 

Failed to execute RAMCode for RAM check!

 

 

Here is the whole debugging message:

SEGGER J-Link GDB Server V6.00b Command Line Version

 

 

JLinkARM.dll V6.00b (DLL compiled Jul 27 2016 18:18:11)

 

 

-----GDB Server start settings-----

 

GDBInit file:                  none

 

GDB Server Listening port:     2331

 

SWO raw output listening port: 2332

 

Terminal I/O port:             2333

 

Accept remote connection:      localhost only

 

Generate logfile:              off

 

Verify download:               on

 

Init regs on start:            on

 

Silent mode:                   off

 

Single run mode:               on

 

Target connection timeout:     0 ms

 

------J-Link related settings------

 

J-Link Host interface:         USB

 

J-Link script:                 none

 

J-Link settings file:          none

 

------Target related settings------

 

Target device:                 STM32L031G6

 

Target interface:              SWD

 

Target interface speed:        1000kHz

 

Target endian:                 little

 

 

Connecting to J-Link...

 

J-Link is connected.

 

Firmware: J-Link Lite-Cortex-M V8 compiled Aug 20 2015 17:57:19

 

Hardware: V8.00

 

S/N: 408000227

 

Checking target voltage...

 

Target voltage: 3.18 V

 

Listening on TCP/IP port 2331

 

Connecting to target...WARNING: T-bit of XPSR is 0 but should be 1. Changed to 1.

 

Connected to target

 

Waiting for GDB connection...Connected to 127.0.0.1

 

Reading all registers

 

Read 4 bytes @ address 0x00000000 (Data = 0x00000000)

 

Read 2 bytes @ address 0x00000000 (Data = 0x0000)

 

Target interface speed set to 1000 kHz

 

WARNING: T-bit of XPSR is 0 but should be 1. Changed to 1.

 

Resetting target

 

Halting target CPU...

 

...Target halted (PC = 0x00000000)

 

R0 = FFFFFFFF, R1 = FFFFFFFF, R2 = FFFFFFFF, R3 = FFFFFFFF

 

R4 = FFFFFFFF, R5 = FFFFFFFF, R6 = FFFFFFFF, R7 = FFFFFFFF

 

R8 = FFFFFFFF, R9 = FFFFFFFF, R10= FFFFFFFF, R11= FFFFFFFF

 

R12= FFFFFFFF, R13= 00000000, MSP= 00000000, PSP= FFFFFFFC

 

R14(LR) = FFFFFFFF, R15(PC) = 00000000

 

XPSR F1000000, APSR F0000000, EPSR 01000000, IPSR 00000000

 

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

 

Reading all registers

 

Read 4 bytes @ address 0x00000000 (Data = 0x00000000)

 

Read 2 bytes @ address 0x00000000 (Data = 0x0000)

 

Select auto target interface speed (2000 kHz)

 

Flash breakpoints enabled

 

Semi-hosting enabled (Handle on BKPT)

 

Semihosting I/O set to TELNET Client

 

SWO disabled succesfully.

 

SWO enabled succesfully.

 

Read 4 bytes @ address 0x00000000 (Data = 0x00000000)

 

Read 2 bytes @ address 0x00000000 (Data = 0x0000)

 

Downloading 192 bytes @ address 0x08000000 - Verified OK

 

Downloading 4072 bytes @ address 0x080000C0 - Verified OK

 

Downloading 36 bytes @ address 0x080010A8 - Verified OK

 

Downloading 4 bytes @ address 0x080010CC - Verified OK

 

Downloading 4 bytes @ address 0x080010D0 - Verified OK

 

Downloading 4 bytes @ address 0x080010D4 - Verified OK

 

ERROR: Timeout while checking target RAM, RAMCode did not respond in time

 

Failed to prepare for programming.

 

Failed to execute RAMCode for RAM check!

 

Writing register (PC = 0xa0020008)

 

Read 4 bytes @ address 0x080002A0 (Data = 0x00000000)

 

WARNING: T-bit of XPSR is 0 but should be 1. Changed to 1.

 

Resetting target

 

Halting target CPU...

 

...Target halted (PC = 0x00000000)

 

Read 2 bytes @ address 0x08000F2E (Data = 0x0000)

 

Read 2 bytes @ address 0x08000F2E (Data = 0x0000)

 

Read 2 bytes @ address 0x08000F2E (Data = 0x0000)

 

R0 = FFFFFFFF, R1 = FFFFFFFF, R2 = FFFFFFFF, R3 = FFFFFFFF

 

R4 = FFFFFFFF, R5 = FFFFFFFF, R6 = FFFFFFFF, R7 = FFFFFFFF

 

R8 = FFFFFFFF, R9 = FFFFFFFF, R10= FFFFFFFF, R11= FFFFFFFF

 

R12= FFFFFFFF, R13= 00000000, MSP= 00000000, PSP= FFFFFFFC

 

R14(LR) = FFFFFFFF, R15(PC) = 00000000

 

XPSR F1000000, APSR F0000000, EPSR 01000000, IPSR 00000000

 

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

 

Reading all registers

 

Read 4 bytes @ address 0x00000000 (Data = 0x00000000)

 

Read 2 bytes @ address 0x00000000 (Data = 0x0000)

 

Setting breakpoint @ address 0x08000F2E, Size = 2, BPHandle = 0x0001

 

Starting target CPU...

 

WARNING: T-bit of XPSR is 0 but should be 1. Changed to 1.

 

...Target halted (DBGRQ, PC = 0xFFFFFFFE)

 

Reading all registers

 

Read 4 bytes @ address 0xFFFFFFFE (Data = 0x061AF9D0)

 

Read 2 bytes @ address 0xFFFFFFFE (Data = 0x0000)

 

Removing breakpoint @ address 0x08000F2E, Size = 2

 

Read 4 bytes @ address 0xFFFFFFFC (Data = 0x000000B1)

 

Read 4 bytes @ address 0xFFFFFFF8 (Data = 0x00000005)

 

Read 4 bytes @ address 0x00000004 (Data = 0x00000000)

 

Read 4 bytes @ address 0xFFFFFFFC (Data = 0x000000B1)

 

Read 4 bytes @ address 0xFFFFFFF4 (Data = 0x00000010)

 

Read 4 bytes @ address 0xFFFFFFF4 (Data = 0x00000010)

 

Read 4 bytes @ address 0x00000010 (Data = 0x00000000)

 

Read 4 bytes @ address 0xFFFFFFFC (Data = 0x000000B1)

 

Read 4 bytes @ address 0xFFFFFFF4 (Data = 0x00000010)

 

Read 4 bytes @ address 0x0000000C (Data = 0x00000000)

 

Read 4 bytes @ address 0x0000000C (Data = 0x00000000)

 

Read 4 bytes @ address 0xFFFFFFF4 (Data = 0x00000010)

 

Read 4 bytes @ address 0x0000000C (Data = 0x00000000)

 

Read 4 bytes @ address 0x00000000 (Data = 0x00000000)

 

Read 4 bytes @ address 0xFFFFFFFC (Data = 0x000000B1)

 

Read 4 bytes @ address 0xFFFFFFF4 (Data = 0x00000010)

 

Read 4 bytes @ address 0x0000000C (Data = 0x00000000)

 

Read 4 bytes @ address 0xFFFFFFFC (Data = 0x000000B1)

 

Read 4 bytes @ address 0xFFFFFFF4 (Data = 0x00000010)

 

Read 4 bytes @ address 0x0000000C (Data = 0x00000000)

 

Read 4 bytes @ address 0xFFFFFFFF (Data = 0x00000000)

I tried to find a solution but unfortunately couldn't find any. Any help please?

Thanks,

Bien

#stm32l031 #flashing-stm32
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
slimen
Senior
Posted on September 14, 2016 at 12:00

Hi,

Which version of J-Link are you using? You can refer to this J-Link 

https://www.segger.com/downloads/jlink/ReleaseNotes_JLink.html

, to have idea on which J-Link version supports STM32L031xx series devices and should be used.

Have a look to this

http://forum.segger.com/index.php?page=Thread&threadID=2635

 with similar issue, it maybe helpful for you.

Regards