2012-10-10 12:25 AM
Hello,
currently I'm evaluating the internal temperature senor of the STM32L151, but in the docs are different values for trimming values given. Sometimes 90° is stated somtimes 110°, so which value is correct? STM32L151xx datasheet -> 110° for upper factory trimming value STM32L151xx errata -> 90° RM0038 reference manual -> 90° regards thomas2012-10-10 7:05 AM
In fact it doesn't matter. The relevant advice from the user manual is:
To reduce the temperature sensor error, the user can measure it at ambient temperature(25°C) to redefine more accurately the average slope (avg_slope) and the offset. The temperature sensor has an offset that varies from one processor to another, so each processor needs to be calibrated. If your design is for a production run, an external temperature sensor with less variation in offset might be more suitable. Cheers, Hal
2012-10-15 4:54 PM
I just received an email from ST stating:
I have preliminary information from our factory, and it appears STM32Ls high density such as yours have correctly programmed engineering data only starting from revision Y (newer than your revision Z).
All previous revisions are susceptible to bad engineering data programming.
(I'm using STM32L152VC)2012-10-16 6:28 AM
Now we just have to figure out the algorithm difference between ''
correctly programmed engineering data
'' and''bad engineering data programming''.
STOne - What is the design slope and offset for Revision Z ? Is there a way that Revision C can be used to measure internal temperature ? If all else fails, with Rev C use actual readings with the processor in a plastic bag in ice water, then at room temperature, then in your expected usage environment with a thermometer nearby. For production, you should switch to Rev Z. Cheers, Hal