2012-02-18 9:26 PM
Hi,
I am using Codesourcery gcc to build the stm32l-discovery demo. I get the following linking error ./Debug/src_icc_measure_Ram.o: In function `EnterLPRUNModeRAM': C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:109: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:109: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:109: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:109: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:110: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:110: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:110: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:110: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:111: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:111: relocation truncated to fit: R_ARM_THM_CALL against `__NOP' C:/CodeLite-embed/msys/home/Projects/Stm32f1L_Discovery_demo/App/src/icc_measure_Ram.c:111: additional relocation overflows omitted from the output collect2: ld returned 1 exit status mingw32-make.exe[1]: *** [Debug/App.elf] Error 1 On investigation this is a result of having an array of __NOP() macro calls which are defined in cm3.h as static __INLINE void __NOP() { __ASM volatile (''nop''); } One __NOP() works ok but if one has two or more a linker error is generated. I have got the program to work by changing the code from do{ __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); __NOP(); } while((USERBUTTON_GPIO_PORT->IDR & USERBUTTON_GPIO_PIN) == 0); to do{ { __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); } { __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); } { __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); } { __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); } { __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); } { __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); } { __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); } { __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); __ASM volatile (''nop''); } } while((USERBUTTON_GPIO_PORT->IDR & USERBUTTON_GPIO_PIN) == 0); There is a similar problem with the __WFE(); macro. One is ok but two in succession fail Again the solution is to use { __ASM volatile (''wfe''); } The bizarre thing is that the Atollic gcc compiler does not give any errors. In addition to the above the code in this demo produces a host of warnings which indicates very lazy and sloppy programming. Atollic's solution seems to be to turn the warnings off. Best regards, Noel Diviney.2012-11-28 7:30 AM
Thank u, it works..
andwhy others
do not experience
this problem
?? Best Regards Lutfi_Indonesia2012-11-28 7:49 AM
__NOP is not actually a function called, but one of the intrinsics supplied by the ARM header files (core_cmInstr.h in this case).
If you check that file, you will notice that this intrinsics are multiply defined, one definition for every toolchain/compiler. Check that your make file / project settings define the proper toolchain macro. For Codesourcery, this is __GNUC__, IMHO.2012-11-28 7:59 AM
and
why others
do not experience
this problem
?? Probably because frankly a lot of people use more professional tools that explicitly target embedded code. GNU/GCC is a more general solution, and while powerful it has many options which are mostly hidden when you code in an IDE, and just press a button. The problem described above seems to be one of the compiler failing to actually INLINE the code properly and doing a NEAR call to a subroutine that subsequently goes out of scope when the linker tries to resolve the calls. You'd have to look at what compiler/linker version and options were doing to understand what was happening with the toolchains that worked vs did not. The STM32L-Discovery project is supplied in an IAR/EWARM only format, along with all the quirks of that specific tool chain.