cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7x3 datasheet and Flash memory programming

Uwe Bonnes
Chief
Posted on March 13, 2018 at 23:04

Hello,

DS12110 rev. 3 in table 51 .' Flash memory programming (single bank configuration nDBANK=1)' misses values for sector erase time with parallelisme x32 and misses even an entry for parallesim x64.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on March 16, 2018 at 17:18

Hello

Bonnes.Uwe

,

You are right, there is a missing values for '

sector (128 KB) erase time':

- Program/erase parallelism x 32 :

typ = 1,1 and max = 2,2

-Program/erase parallelism x 64 :

typ = 1 and max = 2

The missing values will be added

in next release of H7 datasheets.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen