Skip to main content
Associate
December 16, 2023
Question

STM32H753 interface with an external ADC / Ads127l01 / 512ksps / 24bit ADC IEPE / ICP Vibration Data

  • December 16, 2023
  • 0 replies
  • 1779 views

Hello All !

I am a Mechanical Engineer and totally new to STM32; but the assortment of attractive features on these boards tempted me to get one and start my Project. I need to interface a DAQ for IEPE Sensors. I found found one on AliExpress, similar to the TI Evaluation Board they have on public domain, the TIDA-01471 using the TI ADS127L01 ADC. The DAQ has a SPI output. PDF is attached herewith. The same has a Header of 22 pins. Pins are as;

VIN

1

2

VIN

GND

3

4

GND

OUT-F

5

6

SOUR-EN

S-SYNC

7

8

S-DIN

S-SCLK

9

10

OSR0

OSR1

11

12

START

DRDY

13

14

DOUT

DIN

15

16

nCS

SCLK

17

18

GND

RST

19

20

HR

PGA-2

21

22

PGA-1

Pins relevant to ADC are 10, 11, 12, 13, 14, 15, 16, 17, 19, 20, 21 & 22.

Presently do not have the board either; it is on it's way. Just planning it. A word document is also attached whereby I have been sorting out the solution matrix. Please correct me where I have erred.

Never used a STM32 board before but I am an avid learner. Therefore would need all help and patience from the friends. To begin with, can someone please help with the idea that TIMERS / INTERRUPTS also need to be involved in mapping the above parameters within the STM32 ? How many TIMERS and their sequence. I am unable to work it out at the moment. 

Enough for the moment. Thank you all for the audience.

Sincerely,

Muhammad

 

 

This topic has been closed for replies.