2025-05-27 10:36 AM
Dear all;
I have a *** question but it dont work can we have quantity 2 different i2c bus
1 is reconized but not the second bus
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_LTDC_Init();
MX_QUADSPI_Init();
MX_FMC_Init();
MX_I2C2_Init();
MX_I2C4_Init();
MX_SPI1_Init();
MX_UART4_Init();
MX_USART1_UART_Init();
MX_TIM3_Init();
MX_DMA2D_Init();
/* USER CODE BEGIN 2 */
int P=10000;
HAL_TIM_PWM_Start(&htim3,TIM_CHANNEL_4);
//htim3.Instance->CCR1=50;
__HAL_TIM_SET_COMPARE(&htim3,TIM_CHANNEL_4, P);
HAL_StatusTypeDef result;
uint8_t i;
for (i=1; i<128; i++)
{
/* * the HAL wants a left aligned i2c address
* &hi2c1 is the handle
* (uint16_t)(i<<1) is the i2c address left aligned
* retries 2
* timeout 2*/
//ret = HAL_I2C_IsDeviceReady(&hi2c2, (uint16_t)(i<<1), 3, 5);
result = HAL_I2C_IsDeviceReady(&hi2c2, (uint16_t)(i<<1), 3, 5);
if (result != HAL_OK) // HAL_ERROR or HAL_BUSY or HAL_TIMEOUT
{
printf("."); // No ACK received at that address
}
if (result == HAL_OK)
{
printf("0x%X", i); // Received an ACK at that address
}
}
printf("\r\n");
HAL_StatusTypeDef result2;
uint8_t z;
for (z=1; z<128; z++)
{
/** the HAL wants a left aligned i2c address
* &hi2c1 is the handle
* (uint16_t)(i<<1) is the i2c address left aligned
* retries 2
* timeout 2
*/
//ret = HAL_I2C_IsDeviceReady(&hi2c2, (uint16_t)(i<<1), 3, 5);
result2 = HAL_I2C_IsDeviceReady(&hi2c4, (uint16_t)(z<<1), 3, 5);
if (result2 != HAL_OK) // HAL_ERROR or HAL_BUSY or HAL_TIMEOUT
{
printf("."); // No ACK received at that address
}
if (result2 == HAL_OK)
{
printf("0x%X", z); // Received an ACK at that address
}
}
printf("\r\n");
2025-05-27 11:45 AM
Common issues with I2C:
If you have a logic analyzer, look at SDA/SCL signals.
2025-05-27 11:51 AM
What might help is the initialization code, and a schematic/wiring diagram or exactly what you've built.
What device is connected to I2C4 ? What address is it supposed to respond at ?
Is the issue with the Slave or the Master? You're just showing code probing the address space.
2025-05-28 1:09 AM
Thanks for reply That 's really strange i dont understand it's not the first time that occur
It's a compile error :
#include "i2c.h"
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
I2C_HandleTypeDef hi2c2;
I2C_HandleTypeDef hi2c4;
/* I2C2 init function */
void MX_I2C2_Init(void)
{
/* USER CODE BEGIN I2C2_Init 0 */
/* USER CODE END I2C2_Init 0 */
/* USER CODE BEGIN I2C2_Init 1 */
/* USER CODE END I2C2_Init 1 */
hi2c2.Instance = I2C2;
hi2c2.Init.Timing = 0x009034B6;
hi2c2.Init.OwnAddress1 = 0;
hi2c2.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c2.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c2.Init.OwnAddress2 = 0;
hi2c2.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c2.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c2.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c2) != HAL_OK)
{
Error_Handler();
}
/** Configure Analogue filter
*/
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c2, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
{
Error_Handler();
}
/** Configure Digital filter
*/
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c2, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C2_Init 2 */
/* USER CODE END I2C2_Init 2 */
}
/* I2C4 init function */
void MX_I2C4_Init(void)
{
/* USER CODE BEGIN I2C4_Init 0 */
/* USER CODE END I2C4_Init 0 */
/* USER CODE BEGIN I2C4_Init 1 */
/* USER CODE END I2C4_Init 1 */
hi2c4.Instance = I2C4;
hi2c4.Init.Timing = 0x009034B6;
hi2c4.Init.OwnAddress1 = 0;
hi2c4.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c4.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c4.Init.OwnAddress2 = 0;
hi2c4.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c4.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c4.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c4) != HAL_OK)
{
Error_Handler();
}
/** Configure Analogue filter
*/
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c4, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
{
Error_Handler();
}
/** Configure Digital filter
*/
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c4, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C4_Init 2 */
/* USER CODE END I2C4_Init 2 */
}
void HAL_I2C_MspInit(I2C_HandleTypeDef* i2cHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
if(i2cHandle->Instance==I2C2)
{
/* USER CODE BEGIN I2C2_MspInit 0 */
/* USER CODE END I2C2_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2C2;
PeriphClkInitStruct.I2c123ClockSelection = RCC_I2C123CLKSOURCE_D2PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
__HAL_RCC_GPIOH_CLK_ENABLE();
/**I2C2 GPIO Configuration
PH4 ------> I2C2_SCL
PH5 ------> I2C2_SDA
*/
GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF4_I2C2;
HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
/* I2C2 clock enable */
__HAL_RCC_I2C2_CLK_ENABLE();
/* USER CODE BEGIN I2C2_MspInit 1 */
/* USER CODE END I2C2_MspInit 1 */
}
else if(i2cHandle->Instance==I2C4)
{
/* USER CODE BEGIN I2C4_MspInit 0 */
/* USER CODE END I2C4_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2C4;
PeriphClkInitStruct.I2c4ClockSelection = RCC_I2C4CLKSOURCE_D3PCLK1;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
__HAL_RCC_GPIOD_CLK_ENABLE();
/**I2C4 GPIO Configuration
PD12 ------> I2C4_SCL
PD13 ------> I2C4_SDA
*/
GPIO_InitStruct.Pin = GPIO_PIN_12|GPIO_PIN_13;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF4_I2C4;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/* I2C4 clock enable */
__HAL_RCC_I2C4_CLK_ENABLE();
/* USER CODE BEGIN I2C4_MspInit 1 */
/* USER CODE END I2C4_MspInit 1 */
}
}
void HAL_I2C_MspDeInit(I2C_HandleTypeDef* i2cHandle)
{
if(i2cHandle->Instance==I2C2)
{
/* USER CODE BEGIN I2C2_MspDeInit 0 */
/* USER CODE END I2C2_MspDeInit 0 */
/* Peripheral clock disable */
__HAL_RCC_I2C2_CLK_DISABLE();
/**I2C2 GPIO Configuration
PH4 ------> I2C2_SCL
PH5 ------> I2C2_SDA
*/
HAL_GPIO_DeInit(GPIOH, GPIO_PIN_4);
HAL_GPIO_DeInit(GPIOH, GPIO_PIN_5);
/* USER CODE BEGIN I2C2_MspDeInit 1 */
/* USER CODE END I2C2_MspDeInit 1 */
}
else if(i2cHandle->Instance==I2C4)
{
/* USER CODE BEGIN I2C4_MspDeInit 0 */
/* USER CODE END I2C4_MspDeInit 0 */
/* Peripheral clock disable */
__HAL_RCC_I2C4_CLK_DISABLE();
/**I2C4 GPIO Configuration
PD12 ------> I2C4_SCL
PD13 ------> I2C4_SDA
*/
HAL_GPIO_DeInit(GPIOD, GPIO_PIN_12);
HAL_GPIO_DeInit(GPIOD, GPIO_PIN_13);
/* USER CODE BEGIN I2C4_MspDeInit 1 */
/* USER CODE END I2C4_MspDeInit 1 */
}
}
2025-05-28 1:12 AM
here is the error:
09:10:33 **** Incremental Build of configuration Debug for project STM32h743_i2cscan ****
make -j24 all
arm-none-eabi-gcc "../Core/Src/main.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DDEBUG -DUSE_PWR_LDO_SUPPLY -DUSE_HAL_DRIVER -DSTM32H743xx -c -I../Core/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc -I../Drivers/STM32H7xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../Drivers/CMSIS/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -MMD -MP -MF"Core/Src/main.d" -MT"Core/Src/main.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Core/Src/main.o"
../Core/Src/main.c: In function 'main':
../Core/Src/main.c:134:3: warning: implicit declaration of function 'MX_I2C4_Init'; did you mean 'MX_I2C2_Init'? [-Wimplicit-function-declaration]
134 | MX_I2C4_Init();
| ^~~~~~~~~~~~
| MX_I2C2_Init
../Core/Src/main.c:188:52: error: 'hi2c4' undeclared (first use in this function); did you mean 'hi2c2'?
188 | result2 = HAL_I2C_IsDeviceReady(&hi2c4, (uint16_t)(z<<1), 3, 5);
| ^~~~~
| hi2c2
../Core/Src/main.c:188:52: note: each undeclared identifier is reported only once for each function it appears in
../Core/Src/main.c:199:23: warning: implicit declaration of function 'SDRAM_InitSequence' [-Wimplicit-function-declaration]
199 | SDRAM_InitSequence();
| ^~~~~~~~~~~~~~~~~~
make: *** [Core/Src/subdir.mk:67: Core/Src/main.o] Error 1
"make -j24 all" terminated with exit code 2. Build might be incomplete.
09:10:34 Build Failed. 2 errors, 2 warnings. (took 611ms)I don't understand why Hal inicialise the first i2c and not i2c4
2025-05-29 1:56 PM
It looks like the source files that are compiled are out of sync with what you see in the IDE.
Make sure all files are saved, then refresh (F5).
2025-05-29 2:04 PM
It's like you've split the code into different files, and main.c has no reference too the instances or functions.