2024-08-12 3:41 PM
I am trying to implement an IAP function on stm32h563 with Keil. I have a bootloader and image A and B, all running on flash. Image A and image B are running on bank 1 and 2. When i was running image A and updating image B, new image B is successfully programmed in flash and passed software CRC-16 check.
Then I jumped to image B and image B get stuck at the software CRC-16 check. Because I need to read data from flash and flash is somehow locked, and PC goes to a wrong place (like calling an uninitialized pointer).
The flash keeps locked even if I download my firmware again. I can only unlock the flash by erasing the whole flash via Keil IDE and reprogram the bootloader.
I use the ST sample API to erase and write flash. Below is my code of flash operation. Could anyone help me?
/**
* @brief Gets the bank of a given address
* @PAram Address: Address of the FLASH Memory
* @retval The bank of a given address
*/
static uint32_t GetBank(int32_t Address)
{
uint32_t bank = 0;
if (READ_BIT(FLASH->OPTSR_CUR, FLASH_OPTSR_SWAP_BANK) == 0)
{
/* No Bank swap */
if (Address < (FLASH_BASE + FLASH_BANK_SIZE)) // hardfault here
{
bank = FLASH_BANK_1;
}
else
{
bank = FLASH_BANK_2;
}
}
else
{
/* Bank swap */
if (Address < (FLASH_BASE + FLASH_BANK_SIZE))
{
bank = FLASH_BANK_2;
}
else
{
bank = FLASH_BANK_1;
}
}
return bank;
}
/**
* @brief Gets the sector of a given address
* @PAram Address: Address of the FLASH Memory
* @retval The sector of a given address
*/
static uint32_t GetSector(uint32_t Address)
{
uint32_t sector = 0;
if(Address > (FLASH_BASE + FLASH_SIZE_DEFAULT) || Address < FLASH_BASE)
{
sector = OUT_OF_RANGE_SECTOR; // out of range
return sector;
}
if (Address < (FLASH_BASE + FLASH_BANK_SIZE)) // hardfault here
{
sector = (Address - FLASH_BASE)/FLASH_SECTOR_SIZE;
}
else
{
sector = (Address - FLASH_BASE)/FLASH_SECTOR_SIZE;
}
return sector;
}
/*
* Erase @numOfSector sectors in flash from @dstAddr.
* The function will check in which sector @dstAddr locates and erase from the beginning of that sector
*/
HAL_StatusTypeDef flash_sector_erase_only(uint32_t dstAddr, uint8_t numOfSector)
{
uint32_t startSector, BankNumber;
HAL_StatusTypeDef status;
/* Disable instruction cache prior to internal cacheable memory update */
if (HAL_ICACHE_Disable() != HAL_OK)
{
Error_Handler();
}
/* Unlock the Flash to enable the flash control register access *************/
HAL_FLASH_Unlock();
startSector = GetSector(dstAddr);
BankNumber = GetBank(dstAddr);
if(numOfSector == 0 || startSector + numOfSector > OUT_OF_RANGE_SECTOR)
{
return kStatus_InvalidArgument;
}
else
{
/* Fill EraseInit structure*/
EraseInitStruct.TypeErase = FLASH_TYPEERASE_SECTORS;
EraseInitStruct.Banks = BankNumber;
EraseInitStruct.Sector = startSector;
EraseInitStruct.NbSectors = numOfSector;
status = HAL_FLASHEx_Erase(&EraseInitStruct, &SectorError);
}
HAL_FLASH_Lock();
/* Re-enable instruction cache */
if (HAL_ICACHE_Enable() != HAL_OK)
{
Error_Handler();
}
return status;
}
/*
* Write a single flash page from @srcAddr to @dstAddr without erasing it.
* The function will check in which page @dstAddr locates and erase from the beginning of that page.
* Only support quad word write(128 bit)
*/
void flash_bytes_write(uint32_t dstAddr, uint8_t* srcAddr, uint32_t length)
{
int ret=0;
/* Disable instruction cache prior to internal cacheable memory update */
if (HAL_ICACHE_Disable() != HAL_OK)
{
Error_Handler();
}
HAL_FLASH_Unlock();
for(uint32_t i = 0; i<length; i+=16)
{
ret = HAL_FLASH_Program(FLASH_TYPEPROGRAM_QUADWORD, dstAddr + i, (uint32_t)(srcAddr + i));
}
HAL_FLASH_Lock();
/* Re-enable instruction cache */
if (HAL_ICACHE_Enable() != HAL_OK)
{
Error_Handler();
}
}