cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F769I-Discovery - upload to QSPI Flash from uSD card, and display on LCD

john doe
Lead
Posted on April 29, 2017 at 15:37

To prove a bad thing can get worse, I stitched together some of the HAL example code

This project takes RGB8888 bitmaps [max of 25] and uploads them to the QSPI Flash on-board. It outputs information on uart 1

https://github.com/ProjectsByJRP/uSDcard_to_QSPI_flash

 

This project takes the bitmaps in the QSPI flash and displays them on the on-board LCD. output on uart1

https://github.com/ProjectsByJRP/QSPI_Flash_to_LCD

 
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0