cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746V

nigelh
Associate II
Posted on November 09, 2016 at 14:40

Can anybody point me at a document for the the pin configuration for the 'F746 100 pin package. I can't find LCD_B1 on the data sheet or in the reference manual. I assume there is something else as the 'how to configure' information is a bit thin on the ground.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User
Posted on November 09, 2016 at 15:18

> Can anybody point me at a document for the the pin configuration for the 'F746 100 pin package. I can't find LCD_B1 on the data sheet or in the reference manual.

Textual search finds it in 'F746 DS rev.4 at PG12 and PJ13 in both tables.

In other words, there is no LCD_B1 in the 100-pin packages.

> I assume there is something else as the 'how to configure' information is a bit thin on the

ground.

I can't think of anything better founded than those tables in DS.

JW
nigelh
Associate II
Posted on November 09, 2016 at 18:51

Thanks. However I think that's a bit unlikely as that is the LCD version of the of the chip. I was reasoning a misprint was more reasonable rather than a error in the silicon.

ST Renegade
Senior
Posted on November 09, 2016 at 23:35

Hey there,

it appears this device supports only RGB666 & RGB565 displays. That's why you can't find them in the DS or RM. Use the STM32CubeMX for this. It will show you, which pins are present etc...

Have a nice day,

Renegade

nigelh
Associate II
Posted on November 10, 2016 at 22:16

Thanks. Good call.