Skip to main content
Bobby Hayes
Associate II
January 26, 2017
Question

STM32F7 QSPI Exit Memory Mapped Mode

  • January 26, 2017
  • 4 replies
  • 4720 views
Posted on January 26, 2017 at 16:00

Hi,

The QSPI peripheral in the STM32F7 is wonderful.  Nice job ST!

One question:  Is there any way to exit memory mapped mode and go back to indirect RX/TX through the HAL driver?

Thanks!

Bobby
    This topic has been closed for replies.

    4 replies

    Bobby Hayes
    Associate II
    January 26, 2017
    Posted on January 26, 2017 at 16:20

    I tried just re-initializing the peripheral, which worked with the additional step of clearing out FMODE before the re-init.  The code below seems to work:  

    /* Stop memory mapped mode */

    QUADSPI->CCR &= (~(QUADSPI_CCR_FMODE));

    /* ReInitialize QuadSPI ------------------------------------------------------ */

    HAL_QSPI_DeInit(&hqspi);

    /* ClockPrescaler set to 2, so QSPI clock = 216MHz / (2+1) = 72MHz */

    hqspi.Init.ClockPrescaler = 2;

    hqspi.Init.FifoThreshold = 4;

    hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_HALFCYCLE;

    hqspi.Init.FlashSize = POSITION_VAL(0x1000000) - 1;

    hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_2_CYCLE;

    hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;

    hqspi.Init.FlashID = QSPI_FLASH_ID_1;

    hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;

    if (HAL_QSPI_Init(&hqspi) != HAL_OK)

    Nesrine M_O
    Associate
    January 26, 2017
    Gln
    ST Employee
    June 8, 2017
    Posted on June 08, 2017 at 18:47

    Hi Bobby,

    There is no need to completely re-initilize the QSPI preipheral. The memory-mapped mode can be deactivated by changing the FMODE bits in the QUADSPI_CCR register when BUSY is cleared. In Memory-mapped mode, BUSY goes high as soon as the first memory-mapped access occurs. Because of the prefetch operations, BUSY does not fall until there is a timeout, there is an abort, or the peripheral is disabled.

    Using the an abort and the HAL library, you can exit out of QSPI memory-mapped mode using the following code:

    if

    (HAL_QSPI_MemoryMapped(&QSPIHandle, &sCommand, &sMemMappedCfg) != HAL_OK)

    {

      Error_Handler();

    }

    /* ... QSPI in memory-mapped mode ... */

    /* Clear busy bit */

    HAL_QSPI_Abort(&QSPIHandle);

    /* WARNING: Do not make any other memory-mapped access (even using debugger) */

    /* Go back to indirect mode */

    if (HAL_QSPI_Command(&QSPIHandle, &sCommand, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK){

      Error_Handler();

    }

    if

    (HAL_QSPI_Receive(&QSPIHandle, aRxBuffer, 1000) != HAL_OK)

    {

      Error_Handler();

    }

    Guillaume
    Matteo Campese
    Visitor II
    June 5, 2018
    Posted on June 05, 2018 at 18:20

    Hi Guillaume,

    I have some problem with the Abort command: I'm able to use HAL Abort function only when the 'OSPI Timeout Activation' is disable and at least one read request is done on the mapped memory.

    If I try to use the Abort function without the above conditions, the function hangs waiting for the Transmission Complete flag to be set:

    /* Wait until the transfer complete flag is set to go back in idle state */

    status = OSPI_WaitFlagStateUntilTimeout(hospi, HAL_OSPI_FLAG_TC, SET, tickstart, hospi->Timeout);

    and after the Timeout (5 seconds default timeout) the function returns

    HAL_ERROR

    .

    Many Thanks!

    Matteo