cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7 Discovery?

mfkfx1
Associate
Posted on September 30, 2014 at 15:43

Hello,

will ST offer a STM32F7 discovery board? If yes, when can we expect it?

Regards
This discussion is locked. Please start a new topic to ask your question.
36 REPLIES 36
randy
Associate II
Posted on July 14, 2015 at 06:58

Hi Mehmood,

      I believe that the folks of Stlink utility, simply forgot to add the proper flash loader to v 3.6. The AIR IDE has its own flash loader but it is unstable. For some reason loading 14MB of graphics data it stops around the middle and that's it, most probably timing out. Historically, Stlink utility is superb when it comes to flashing external memory.  So if any of the ST folks reading this can you add the proper .stldr file for the disco f7 board to external flash loaders in stlink utility v 3.6 ???? As documented.

Regards,

Uwe Bonnes
Chief
Posted on July 15, 2015 at 18:09

LCD_BK_CTRL is on PK3. It is probably active low and not pulled.

markmansell9
Associate
Posted on October 10, 2015 at 23:45

Having read, further down the board, about the problems people have had with ST-Link I thought I'd just say how I managed to re-flash my board with this demo application.

After unpacking the zip, I discovered that the object code was in .hex format. I downloaded Hex2Bin (http://sourceforge.net/projects/hex2bin/?source=typ_redirect) and, tweaked the Makefile, and recompiled for Linux then ran it on the .hex file.

I then plugged in the board, navigated to the mounted directory and copied the bin file generated by Hex2Bin into it.

With one caveat, this was flawless and delightfully simple.

The one problem I hit was that the board originally declared itself to have no space due to a large demo I had previously installed. Just unplugging and re-plugging the USB fixed this.

matthew239955_stm1_st
Associate II
Posted on February 06, 2016 at 20:19

I could not get the MCO1 pin to work on the stm32f7 disco board. I noticed the pin is not enabled in the cube demo code also. Should/Can it work?

If not can anyone recommend the best way to get a fast ( 40+ MHz ) clock output?

timers/spi maybe?

Thanks,

Matt

 

Radosław
Senior III
Posted on February 06, 2016 at 21:02

Check this topic. Errors on schematic and pin discriptions.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F7%20MCO%20problem&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&TopicsView=https%3a//my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/AllItems.aspx&currentviews=44]Link

matthew239955_stm1_st
Associate II
Posted on February 07, 2016 at 12:17

Many thanks. Problem solved.

Ard.D10 is PA8 (not D5)

Posted on June 09, 2018 at 19:32

>>What would be a reason to use STM32F7 device for controlling some low stuff, like then servos and some stupid devices? 

The future calls, and says Flight Controllers

https://oscarliang.com/betaflight-f7-fc/

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..