cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32F4xx] Only 16 GPIO under control?

hjm
Associate II

The STM32F4xx reference manual (RM0090) specifies under the GPIO main features section that there are "up to 16 I/Os under control" - does this mean I cannot control more than 16 GPIO pins or am I interpreting this incorrectly?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
AvaTar
Lead

Where, exactly ?

And if so, it most probably refers to the size of one GPIO port.

The F4xx RefManual describes GPIO ports "numbered" from A to K, i.e. 11.

hjm
Associate II

Each bank supports 16 pins, this design is then replicated across multiple banks, A thru K, perhaps more or less usable depending on package

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..