cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4xx Example code bug?

Anderson.Steven
Associate
Posted on October 13, 2015 at 15:32

In file: 

...\STM32F4xx_DSP_StdPeriph_Lib_V1.6.0\Project\STM32F4xx_StdPeriph_Examples\ADC\ADC_TripleModeInterleaved\main.c

Is DMA_Memory0BaseAddr really intended to be a pointer to a pointer?

The variable aADCTripleConvertedValue is an array of 3 uint32_t's, so should (uint32_t)&aADCTripleConvertedValue below need a ''[0]'' appended?

From the file:

Declaration:

/* Private variables ---------------------------------------------------------*/

__IO uint32_t aADCTripleConvertedValue[3];

Use:

  DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&aADCTripleConvertedValue;

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on October 13, 2015 at 18:16

Actually, all three of these resolve to the same address

DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)aADCTripleConvertedValue;

DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&aADCTripleConvertedValue;

DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&aADCTripleConvertedValue[0];

I'd prefer case 3, over 1, but I think you'll find there are all valid.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..