cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4Discovery + DCMI + OV7660 (OV7670)

jeno
Associate II
Posted on July 21, 2013 at 18:42

The original post was too long to process during our migration. Please click on the attachment to read the original post.
20 REPLIES 20
armindavatgaran
Associate III
Posted on August 08, 2015 at 09:41

Hello

Finally it is done, the images are captured with 174 * 144 resolution in YUV4:2:2 and 172 * 144 in RGB565 mode.

Now i'm configuring it for proper color output.

Thanks.