2015-10-04 6:16 AM
Hello!
I'm trying to run STemWin/FreeRTOS/HAL on STM32F429IG revision Y at 168MHz.SDRAM (IS42S16400J-7TLI) connected to FMC controller and runs fine by itself (CAS_LATENCY_3/CLOCK_PERIOD_2/RBURST_ENABLE/RPIPE_DELAY_1).TFT display (AT070TN92, 800x600 RGB888) connected to LTDC and framebuffer set to SDRAM addresses. TFT clock is 24MHz. With my parameters set to LDTC I can see ~42Hz on VSYNC pin. Frame buffer addresses is 0xd0000000 and 0xd0200000.OK, forget for now about STemWin, just configure layers and place some data to framebuffer.ARGB888/ARGB8888 - lost syncRGB888/ARGB8888 - runs fine.OK, now I will modify framebuffer contents in main() loop while looking on screen.ARGB8888/ARGB8888 - lost syncRGB888/ARGB8888 - lost syncRGB888/RGB888 - lost syncRGB888/RGB565 - runs fine...What? Why writing to SDRAM by CPU breaks LTDC DMA transfers??OK, let's try to write to framebuffer with DMA2D.ARGB8888/ARGB8888 - lost syncRGB888/ARGB8888 - lost syncRGB888/RGB888 - lost syncRGB888/RGB565 - lost syncRGB565/RGB565 - runs fine...It is going even worse than CPU.If I turn on STemWin with DMA2D transfers in LCD_DEVFUNC_FILLRECT, I can run only one layer of RGB565.As I understand, DMA2D tries to copy to SDRAM and LTDC cannot get data from SDRAM when needed to paint next line and then sync losts. I can see it as chaotically shifting image to right/left.What should I do with this? Can I set highest priority to LTDC transfers, so DMA2D and CPU will access to SDRAM only when it is not needed to LTDC?Maybe I have missed something?Thanks!2018-12-21 3:26 PM
Yes, you have missed Table 10, from the document https://www.st.com/resource/en/application_note/dm00287603.pdf