cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32f427vit6 replacement

DSmit.111
Associate II

Can i replace the stm32f427vit6 with the f429vit6, f437vit6 or 439vit6 without changing code, and are they completely pin compatible?​

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Yes. The F429 and F439 have LCD. The F437 and F439 have crypto. The F427 has neither of these but is otherwise identical.

The "List Pinout Compatible MCUs" feature in CubeMX can be used to answer questions like these.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
TDK
Super User

Yes. The F429 and F439 have LCD. The F437 and F439 have crypto. The F427 has neither of these but is otherwise identical.

The "List Pinout Compatible MCUs" feature in CubeMX can be used to answer questions like these.

If you feel a post has answered your question, please click "Accept as Solution".

Thanks you 👍🏻