cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F412 Multiple PWM Control Inquiry

KOPRO
Associate III

I am developing a product using the STM32F412REFxLQFP64 chip, and I want to implement multi-PWM control.

 

For TIM2 buzzer control: TIM_HandleTypeDef TIM2 PB10 ------> TIM2_CH3

 

TIM3 is used to generate a 1kHz waveform: TIM_HandleTypeDef TIM3 Channel 4 PB1 ------> TIM3_CH4

void buzzerInit(void)
{
	Buzzer_InitTypeDef buzzerConfig;
	buzzerConfig.channel = TIM_CHANNEL_3;
	buzzerConfig.timer = &htim2;
	buzzerConfig.timerClockFreqHz = HAL_RCC_GetPCLK2Freq(); // NOTE: this should be freq of timer, not frequency of peripheral clock
	hbuzzer.Init = buzzerConfig;
}
void buzzer(BUZZER_StateTypeDef mode){
	buzzerStart(&hbuzzer);
	size_t songSize;
	switch(mode){
		case BUZZER_REGISTER:{
			songSize = sizeof(buzzer_register_theme) / sizeof(buzzer_register_theme[0]);
			for (size_t i = 0; i < songSize; i++) {
				buzzerNote(&hbuzzer, buzzer_register_theme[i].pitch);
				HAL_Delay(buzzer_register_theme[i].duration * 15);
			}
			break;
		}
		case BUZZER_START:{
			songSize = sizeof(buzzer_start_theme) / sizeof(buzzer_start_theme[0]);
			for (size_t i = 0; i < songSize; i++) {
				buzzerNote(&hbuzzer, buzzer_start_theme[i].pitch);
				HAL_Delay(buzzer_start_theme[i].duration * 15);
			}
			break;
		}
		case BUZZER_END:{
			songSize = sizeof(buzzer_end_theme) / sizeof(buzzer_end_theme[0]);
			for (size_t i = 0; i < songSize; i++) {
				buzzerNote(&hbuzzer, buzzer_end_theme[i].pitch);
				HAL_Delay(buzzer_end_theme[i].duration * 15);
			}
			break;
		}
		default :{
			break;
		}
	}
	buzzerStop(&hbuzzer);
	return;
}
void ctrl_pwm_1hz(char _flg)
{
	if(pwm_status == _flg)
		return;
	pwm_status = _flg;
	if(_flg == 0)
	{
		HAL_TIM_PWM_Stop(&htim3, TIM_CHANNEL_4);
	}
	else
	{
		HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_4);
	}

}

When I control the buzzer and the 1kHz signal individually,

 

there are no issues. However, when I try to control them simultaneously,

 

the buzzer does not sound.

 

How can I solve this issue?

 

Thank you.

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

 

Thank you

htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;

I changed this source for activation and it works normally.