cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f407vet6 MCU general questions

Andrew Crawford
Associate II
Posted on April 05, 2018 at 23:35

Hey everyone, I'm new to these microcontrollers and new to these MCUs in general, and had a few questions... First off, i have some experience using Arduinos, so I'm somewhat familiar with the functionality and programming involved, and I've done all the research I can as far as finding the compatible software for programming, and looking more into the arm assembly language involved (in case I need it alongside c), but I wanted to ask more about the capabilities of the board, and whether or not I can do certain things.

The board Ive ordered has a built in SD card reader and claims to have pins supporting an LCD screen, wireless, etc... So I was wondering if it may or may not be possible to run a light version of Linux (with a GUI) off of it, maybe using a Bluetooth keyboard and mouse. The only operating system I've found is the rtos, which definitely seems appealing for its own ease of use and purposes, but I was wondering if these boards were even capable of running anything with a GUI, if optimally configured (or if any such thing may already exist). Thanks!

*As a side note, I'm not necessarily asking if it's already been done, I would just as well be interested in doing it myself, just wondering if the capabilities may or may not potentially be there. Thanks!

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
Andrew Crawford
Associate II
Posted on April 22, 2018 at 03:10

This what I have, more or less (from a different vendor): 

https://m.ebay.com/itm/STM32F407VET6-Development-Board-Core407V-Cortex-M4-STM32-MCU-Full-IO-Expander-SG-/112459621879?_mwBanner=1

 
Andrew Crawford
Associate II
Posted on April 22, 2018 at 03:16

Also, now that I see better details on this product description, I see some pins are dedicated for SPI, i2c, uart, etc, so seems I just need a datasheet for this. But, aside from those limitations as well, could this perhaps be used as an intermediary device between Arduinos? Sorry, just not entirely sure how these work (or what i would even use to program it), I'm just looking to sketch out the details of something that could potentially be a longer project to be done in stages, if possible. Thanks!

T J
Lead
Posted on April 22, 2018 at 03:20

if you have used motors before, you will know about back EMF upsetting the processor.

if you look carefully at the STSPIN32F0  diagram, it will show you what you need to drive a motor.

if you could discuss how many motors you need...

that will point you toward a network solution with a Master, like your STM32F407 board and a bunch of motor drive boards.

CanBus is one solution,Bidirectional, fast, self recovers.

RS485 is about the same thing anyhow,

Rs232 is not really suitable for you since it is point to point.

Just food for thought.

Posted on April 22, 2018 at 02:37

networking first, you have to talk to the steppers.

I would strongly recommend that you use LQFP parts.

the BGA parts will fail after a time due to the vibrations.

the largest LQFP is 208pin,

it is very difficult to use 12 motors from a single processor.

therefore your next decision is about a one or two motor control unit and a network.

there are some 20pin devices for under $1, that could run 1,2,3,4 motors then you need the HighSide drive.

:(

https://www.digikey.com.au/products/en/integrated-circuits-ics/embedded-microcontrollers/685?FV=ffe002ad&quantity=&ColumnSort=1000011&page=1&k=stm32f&pageSize=25

 

there are dedicated ST parts for motor controls, this has it all.

https://www.google.com/url?sa=t&rct=j&q=&esrc=s&source=web&cd=3&ved=0ahUKEwiT-Zyf0czaAhXKurwKHQjwC7cQFghYMAI&url=http%3A%2F%2Fwww.st.com%2Fresource%2Fen%2Ftechnical%2FDM00330483.pdf&usg=AOvVaw0befj7cGJFe92Gs2p1OngX

 
Posted on April 22, 2018 at 03:06

Sorry, I suppose I should have been more specific about what I have/am looking at. I have the microcontroller on a board, and now that I've gotten it (a couple days ago) here's a picture. What would I need to know whether or not this one can use motors?

And what I'm thinking for the overall structure could also possibly be simplied by a simple pin out/in on each end, again using separate Arduinos for each part of the sensors, and if/where the sensors detect something, trigger something a generic pin to output, and I could use this MCU as an intermediary controller to either use motors off itself, or likewise trigger other similar pins to communite back to *another* Arduino. 

I'm just not sure if this can be done. Or in the case of what you addressed, just what I'm looking at. Thanks!

Posted on April 22, 2018 at 03:35

Ah, thanks! I haven't used motors yet, unfortunately, but will be in many future projects, so I'm sure that'll be super helpful, I'll definitely have to look more into that. And I'm not quite sure yet, as I was looking to do something larger over time, so I'll have to look into the former before I have a better idea. As of now just two, for pan and tilt of the sensors mounted onto something, but if I attached an arm (or even could) plus something for mobility, then we'd have to see (again, supposing I even could). So I'll just have to keep doing my research and come back. Thanks!