STM32F407 Timer reampping
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-07-11 2:17 AM
Posted on July 11, 2014 at 11:17
Hello
I'm using the Timer2 as Encoder Position Timer: void Encoder_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_5; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_TIM2); GPIO_PinAFConfig(GPIOA, GPIO_PinSource5, GPIO_AF_TIM2); TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_TimeBaseStructure.TIM_Period = 0xffff; TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); /* Configure the timer */ TIM_EncoderInterfaceConfig(TIM2, TIM_EncoderMode_TI12, TIM_ICPolarity_Rising, TIM_ICPolarity_Falling); TIM_SetCounter (TIM2, (uint32_t) Encoder_Position_Default); //set the Timer to the default init value (middle) /* TIM2 counter enable */ TIM_Cmd(TIM2, ENABLE); TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); } Timer 4 I use to measure a frequency on a second Encoder. This is working great. But in a different seeting I have just 1 Encoder connected to the Timer4 to measure the frequency, works aswell. But I need to get the EncoderPositionMode fro the same Encoder Signals which ones are connected to Timer2. Can I remap the Signals from Timer4 to Timer2 to measure the frequency with Timer4 and the Position with Timer2 without a connected Encoder to the Timer2? Is there an example? Thanks and Regards, Dominik
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-07-11 7:47 AM
Posted on July 11, 2014 at 16:47
If I understand the question correctly, the answer is no.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..