cancel
Showing results for 
Search instead for 
Did you mean: 

[stm32f405rgt6] can't program + connection lost now and then

hotzhao
Associate
Posted on March 25, 2016 at 10:36

I am trying to set up a minimal circuit for stm32f405rgt6 with breadboard and a breakout board.

The problems I have are:

1. I can connect to stm32f405rgt6 via ST-LINK utility, and see the content are all 0xFFFFFFFF starts from 0x08000000. But the connection is very unstable. Sometimes, it could last for like 5 minutes, sometimes, connection lost in a few seconds.

2. While stm32f405rgt6 is connected, I tried to click on ''program & verify''. I could get 2 kinds of errors:

2.1 ''Elf Loader could not be transfered to device''.

2.2 ''Programming error @ 0x08000000''

I am not sure if the unstability is introduced by the breadboard. Do I have to use a PCB?

Or the chip I bought is not good? I only have one stm32f405rgt6 at hand right now.

Here are the detailed connection:

VDD(19,32,48,64) 3.3v

VSS(18,63) ground

VDDA,VBAT 3.3

VSSA ground

I have 10*100nf + 4.7uF between VDD and ground.

2*2.2uF between VCAP_1, VCAP_2 and ground.

BOOT0 ground

NRST,SWCLK,SWDIO connected with CN2(SWD) of the STM32F4-DISCOVERY board.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 25, 2016 at 11:30

Bit of a rats nest there. You have the grounds connected together? And the original target disconnected?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..