cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 waking up from STANDBY by RTC alarm

mchalapetr
Associate II
Posted on May 11, 2015 at 15:27

Hi,

I have a big problem with waking up the STM32F4 MCU from STANDBY mode by RTC alarm and I dont see any solutions...

The problem is that the MCU wakes up only sometimes from the RTC Alarm. Usually like 3 times in a row and then stops. Waking up by user button is fine...

I use LSE and clock itself works fine even when RTC alarm doesnt wake up the MCU...It looks like there is some problem with redefinition of the RTC alarm, possibly some IRQ flags...

I found some topics regarding same problems but reading them all I think that I am doing everything right...

The operation itself should be simple...I manually set up RTC alarm and get to STANDBY mode and after that the MCU wakes up does something and then goes back to STANDBY in a loop until I interupt it manually by button...

Manual set up looks like this:

// Load time and date values from RTC

RTC_AWU_GetDateTime(&time, RTC_AWU_Format_BIN);

// Set up RTC alarm

alarm_time.hours = time.hours;

alarm_time.minutes = time.minutes;

alarm_time.seconds = time.seconds + 5;

alarm_time.alarmtype = RTC_AWU_AlarmType_DayInWeek;

alarm_time.day = 1;

RTC_AWU_SetAlarm(RTC_AWU_Alarm_B, &alarm_time, RTC_AWU_Format_BIN);

/* Power down */

// Disable wakeup pin (BUTTON = PA0)

PWR_WakeUpPinCmd(DISABLE);

// Clear standby/wakeup flag

PWR_ClearFlag(PWR_FLAG_SB | PWR_FLAG_WU);

// Enable wakeup pin (BUTTON = PA0)

PWR_WakeUpPinCmd(ENABLE);

// Go to standby mode

PWR_EnterSTANDBYMode();

Then the loop exacly the same:

// RTC init (PWR_BackupAccessCmd(ENABLE) present here)

RTC_AWU_Init(RTC_AWU_ClockSource_External);

if (RTC_GetITStatus(RTC_IT_ALRB) != RESET){

/*Some code here*/

// Load time and date values from RTC

RTC_AWU_GetDateTime(&time, RTC_AWU_Format_BIN);

// Set up RTC alarm

alarm_time.hours = time.hours;

alarm_time.minutes = time.minutes;

alarm_time.seconds = time.seconds + 5;

alarm_time.alarmtype = RTC_AWU_AlarmType_DayInWeek;

alarm_time.day = 1;

RTC_AWU_SetAlarm(RTC_AWU_Alarm_B, &alarm_time, RTC_AWU_Format_BIN);

/* Power down */

// Disable wakeup pin (BUTTON = PA0)

PWR_WakeUpPinCmd(DISABLE);

// Clear standby/wakeup flag

PWR_ClearFlag(PWR_FLAG_SB | PWR_FLAG_WU);

// Enable wakeup pin (BUTTON = PA0)

PWR_WakeUpPinCmd(ENABLE);

// Go to standby mode

PWR_EnterSTANDBYMode();

}

The RTC_AWU_SetAlarm function looks like this...

// Disable Alarm B

RTC_AlarmCmd(RTC_Alarm_B, DISABLE);

// Disable Alarm B interrupt

RTC_ITConfig(RTC_IT_ALRB, DISABLE);

// Clear Alarm B pending bit

RTC_ClearFlag(RTC_IT_ALRB);

// Clear RTC Alarm pending bit

EXTI_ClearITPendingBit(EXTI_Line17);

// Configure EXTI 17 as interrupt

EXTI_InitStruct.EXTI_Line = EXTI_Line17;

EXTI_InitStruct.EXTI_Mode = EXTI_Mode_Interrupt;

EXTI_InitStruct.EXTI_Trigger = EXTI_Trigger_Rising;

EXTI_InitStruct.EXTI_LineCmd = ENABLE;

EXTI_Init(&EXTI_InitStruct);

// Configure the RTC Alarm Interrupt

NVIC_InitStruct.NVIC_IRQChannel = RTC_Alarm_IRQn;

NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStruct.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStruct);

// Set RTC alarm settings

// Set alarm time

RTC_AlarmStruct.RTC_AlarmTime.RTC_Hours = DataTime->hours;

RTC_AlarmStruct.RTC_AlarmTime.RTC_Minutes = DataTime->minutes;

RTC_AlarmStruct.RTC_AlarmTime.RTC_Seconds = DataTime->seconds;

RTC_AlarmStruct.RTC_AlarmMask = RTC_AlarmMask_DateWeekDay;

etc...

// Configure the RTC Alarm B

RTC_SetAlarm(format, RTC_Alarm_B, &RTC_AlarmStruct);

// Clear Alarm B pending bit

RTC_ClearFlag(RTC_IT_ALRB);

// Enable Alarm B interrupt

RTC_ITConfig(RTC_IT_ALRB, ENABLE);

// Enable Alarm B

RTC_AlarmCmd(RTC_Alarm_B, ENABLE);

Thanks very much for your help...

#rtc #stm32f4 #alarm
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
mchalapetr
Associate II
Posted on May 15, 2015 at 14:38

Hi problem was with this line....alarm_time.seconds = time.seconds + 5;

Basically an overflow of the usable range...I thought that the RTC modifies the data before using...
waclawek.jan
Super User
Posted on May 15, 2015 at 14:56

> Hi problem was with this line....alarm_time.seconds = time.seconds + 5;

Thanks for letting us know, this may help others.

I fought RTC recently too - setting the time to 12h mode (am/pm) then setting hour to 13 allows the clock to run up to 31:59:59... :)

JW