STM32F4 USB hid host - non boot protocol
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-09-16 3:48 PM
Dear All,
Although this is my first post here, I am quite often reading my.st.com forum, when I need to find solution for my problems. Unfortunatley, this time I could not find the answer in existing threads for above problem: I am trying to implement independent controller for multiaxis joystick. The plan is that stm32f4 will act as a ''bridge'' between USB hid and CAN bus. My setup is as in the picture:http://sdey7tkk.home.pl/kreator/data/documents/setup.jpg
I have run mouse and keyboard hid host based on provided by stm examples without any problems. The problem is that library support only boot protocol as I understand, so only mouse- and keyboards-like devices. My multi-axis controller is non boot protocol device. System is initializing ok, device is also recognized and enumerated, results received via uart terminal are as follow:System Initializing... Done! System Ready Device Attached > Low speed device detected VID : 046Dh PID : C626h > HID device connected Manufacturer : 3Dconnexion Product : SpaceNavigator Serial Number : N/A Enumeration done! USBH_USR_UserInput! Device is not supported!
Last message is sent by stm32 after not passing above condition in usbh_hid_core.c src file:
''(...) if(pphost->device_prop.Itf_Desc[0].bInterfaceSubClass == HID_BOOT_CODE) { (...) } else {pphost->usr_cb->DeviceNotSupported();}''
Connected Axis controller is not boot protocol device - it is report protocol device. Its interfece descriptor is stated above:
http://sdey7tkk.home.pl/kreator/data/documents/Urz=C4=85dzenie=20USB=20interfejsu=20HID3d.html
As in report descriptor: data are being sent in 3 reports:
Report ID 01: 3x16 bit values of linear movements (X, Y, Z) Report ID 02: 3x16 bit values of rotational movements (Rx, Ry, Rz) Report ID 03: 1x8 bit value byte buttons state (Button) Report ID 04: 1x8 bit value LED state report send to the device Report IDs 05-11 are never sent in this version of usb device. For better visualisation, below is a screen from USB sniffer application:http://sdey7tkk.home.pl/kreator/data/documents/3d=2002.jpg
Has anyone experience or know how to receive data sent by usb hid non boot protocol device with several report ids?
I think not only me is interested in other than boot protocol hid devices implentation on stm32f4.Best regards and thanks in advance for your help!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-03-07 4:00 AM
Are you to solve the problem of reading full speed USB joystick using stm32 host library? If yes, provide me help,?