cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4, HAL Lib, USART IRQ

tommaso
Associate II
Posted on February 10, 2016 at 09:40

Hi all,

I'm working with STM32F4 mcu and keil uVision 5 IDE. I'm tryng to configure RS232 periph. but I have a problem. Transmission works fine but I'm not able to receive interrupt when something is received. Here my code:


/** Init Rs232 port

*/

void init_RS232(void){

GPIO_InitTypeDef GPIO_InitStruct;


/* GPIO Ports Clock Enable */

__GPIOC_CLK_ENABLE();

__USART3_CLK_ENABLE();


/**USART3 GPIO Configuration

PC10 ------> USART2_TX

PC11 ------> USART2_RX

*/


/*Configure GPIO pin : RS232 Pin */

GPIO_InitStruct.Pin = GPIO_PIN_10 | GPIO_PIN_11; 

GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

GPIO_InitStruct.Pull = GPIO_NOPULL;

GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

GPIO_InitStruct.Alternate = GPIO_AF7_USART3;

HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);


/* Configure USART3 parameters */ 

USART3_Handle.Instance = USART3;

USART3_Handle.Init.BaudRate = 9600;

USART3_Handle.Init.Mode = USART_MODE_TX_RX;

USART3_Handle.Init.Parity = USART_PARITY_NONE;

USART3_Handle.Init.StopBits = USART_STOPBITS_1;

USART3_Handle.Init.WordLength = USART_WORDLENGTH_8B;

HAL_USART_Init(&USART3_Handle);



HAL_USART_Receive_IT(&USART3_Handle, rx_buffer, 16); 

HAL_NVIC_SetPriority(USART3_IRQn, 3, 0);

HAL_NVIC_EnableIRQ(USART3_IRQn); 

}

I would to receive an interrupt every time a char is received and I would like to manage by myself the buffer. With old lib (standard periph lib) I was able to do this. With new HAL ones not. Can you help me? Thanks a lot.
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Amel NASRI
ST Employee
Posted on February 18, 2016 at 10:48

Hi crazy_code,

There is no need to call 

HAL_NVIC_ClearPendingIRQ in the IRQ handler.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.