cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4-Discovery lwIP compilation errors

giannisroussos0
Associate II
Posted on June 05, 2015 at 01:56

Hi,

I have a STM32F4 Discovery + DM-STF4BB and I want to try lwIP on it. I have SW4STM32 installed and I am trying to create a new project through the wizard, using STM32Cube HAL, and lwIP, with and without FreeRTOS.

I have tried many different project creation settings but haven't been able to compile any project succesfuly.

The problems arise from various header files in the stm32f4discovery_hal_lib project that include other header files that either do not exist (eg. ''config.h'' included in Middlewares\Third_Party\LwIP\test\unit\lwip_check.h) or are located in the wrong path (eg. ''lwip/ip_addr.h'' included in Middlewares/Third_Party/LwIP/src/netif/etharp.c)

I have also been trying to find a ready made lwip project for the F4-Discovery I could just import into SW4STM32, but the Projects/STM32F4-Discovery folder does not have any such project.

So, is there an easy way to test lwIP on my dev boards?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
alfredgustav
Associate II

I think you need to manually add the include path in the IDE.

If you use eclipse based IDE, do it under "build setting -> C/C++ general -> paths and symbols -> includes"

3 years without an answer? wow...