Question
STM32F4-Discovery Lowest Possible Power?
Posted on November 03, 2015 at 20:44
I am fully aware of the SM32F407's low-power capabilities. What I was wondering is what are the EVAL kit's low-power capabilities? It seems no matter which mode the MCU is in, I'm forced into drawing ~40mA. It's be nice if I could shut down, jump, (de)solder, something on the Eval kit to get the draw down to ~1mA in standby. Yes, I know that pwr_led is pretty much hardwired direct to 3V, so no matter what I'll be drawing 3mA unless there's something I'm missing.
Anyone have any tricks? #powerconsumption #discovery