cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F334 and high-resolution timer

a1379109
Associate
Posted on August 25, 2014 at 09:27

New STM32F334 have high-resolution timer with 217 ps resolution,

It

's nice,

but

what

real

precision is achieved

when

the timer

used to measure the

time

between

two edges

of the signal applied

to

the processor

GPIO?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Vincent Onde
ST Employee
Posted on March 18, 2015 at 09:58

Hello,

The high-resolution is available solely for waveform generation.

For input capture and period measurement, the external signals are resampled by the internal clock (144MHz). This corresponds to a 6.9ns resolution.

What kind of resolution are you looking for? Is it for a single-shot (instantaneous) or multi-period measurement?

Best regards,

Vincent