cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f303 opamp precision

armindavatgaran
Associate III
Posted on January 14, 2017 at 20:38

Hello

It is mentioned in the stm32f303vc that it's opamp GBW is 8, but as i measured in the lab, the opamp output (i tested opamp 1&2 in follower mode) can't follow a sine wave above 700KHz in frequency, i.e output becomes like triangle wave and above 3MHz, it's amplitude will be filtered also.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0