Skip to main content
Davide Rizzi
Visitor II
October 6, 2017
Question

STM32F303 internal bootloader does not work - pt. II

  • October 6, 2017
  • 0 replies
  • 489 views
Posted on October 06, 2017 at 12:35

Hello everybody,

  I am still having problems with the STM32F303 bootloader.

Description

  • STM32F303CC
  • External 24MHz CMOS oscillator
  • 1.5kohm pullup on USB_DP
  • USB working perfectly (in the application: no issues whatsoever, tens of boards deployed)
  • BOOT0 pin pulled up

On 3 out of 6 boards, the USB does never get enumerated. The boards keep resetting randomly - the reset is software.

On 2/6 boards everything works reliably, while the other board works 'sometimes'.

The HSE ready bit in RCC_CR is 1, and it seems to stay that way (the HSE bypass bit in RCC_CR is 0 - can it be a problem with an external oscillator?).

I have no clues. What I have discovered is that only at times the FW tries to configure the USB - at times it skips it. At times the FW ends in a loop where it keeps resetting the watch dog, at times it ends in a loop where it reads pin status from GPIOA and GPIOD. Most of the times it simply reset.

I cannot find out what causes this reset - all the vectors bring to 0x1fffed10. And, by the way, stepping through asm code can be very tiring. ;)

    This topic has been closed for replies.