2017-02-27 1:07 AM
Hi all, I am using a STM32F302RE MCU with a customised board. My code works find when I run it at normal temperature. However, when I test it at 55 degrees, the code goes to Hard fault handler after the line in the source code is placing data in the pTxMsg pointer's data field. Any reasons why this could be happening or any ways to solve this? I have already tried increasing my stack size but this does not seem to solve the problem. Any help is appreciated!
#stm32 #stm32f302re #stm32f3022017-02-27 1:40 AM
Hi
MK.ShaSha
,-Nesrine-
2017-02-27 4:49 PM
1. MCU PCLK: 20 MHz, VDD: 3.3V
2. Yes, executing from flash memory. I have checked my wait state config and I do not find any issues with them.
3. I have checked the SCB->CFSR register. I have the FORCED bit of hard fault set and INVSTATE of usage handler set.
2017-02-27 7:27 PM
Ok, but why is it faulting on that pointer? Is the pointer invalid? What address is it trying to access? Does that address appear valid/viable? Do you sanity check the pointer before use?
Shouldn't need a wait-state at 20 MHz, does adding one impact things?
Is the issue with the STM32? Could it be a regulator, capacitor, crystal, or something else? How localized is the heat application? Can you apply the heat probe directly/only on the STM32? Can you output the internal clock via MCO?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.