cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F302R8 an error occurs after burning the hex file

bebejjk
Associate

I always get an error after burning the hex file to STM32F302R8. The burning is completed through STM32 ST-LINK Utility. Below is the error log.

16:05:15 : ST-LINK SN : 0664FF515570514867174448
16:05:15 : V2J33M25
16:05:15 : Connected via SWD.
16:05:15 : SWD Frequency = 4,0 MHz.
16:05:15 : Connection mode : Connect Under Reset.
16:05:15 : Debug in Low Power mode enabled.
16:05:16 : Device ID:0x439
16:05:16 : Device flash Size : 64KBytes
16:05:16 : Device family :STM32F301x4-x6-x8/F302x4-x6-x8/F318xx
16:05:23 : Memory programmed in 1s and 594ms.
16:05:23 : Disconnected from device.
16:05:23 : Connection to device is lost: check power supply and debug connection.
16:05:23 : If the target is in low power mode, please enable "Debug in Low Power mode" option from Target->settings menu.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
bebejjk
Associate

Complete error log after trying again.

16:19:29 : ST-LINK SN : 0664FF515570514867174448
16:19:29 : V2J37M26
16:19:29 : Connected via SWD.
16:19:29 : SWD Frequency = 4,0 MHz.
16:19:29 : Connection mode : Connect Under Reset.
16:19:29 : Debug in Low Power mode enabled.
16:19:29 : Device ID:0x439
16:19:29 : Device flash Size : 64KBytes
16:19:29 : Device family :STM32F301x4-x6-x8/F302x4-x6-x8/F318xx
16:19:38 : [stm32motor.hex] opened successfully.
16:19:38 : [stm32motor.hex] checksum : 0x00296C2E
16:19:45 : Memory programmed in 1s and 703ms.
16:19:45 : Verification...OK
16:19:45 : Programmed memory Checksum: 0x00296C2E
16:19:46 : Disconnected from device.
16:19:46 : Connection to device is lost: check power supply and debug connection.
16:19:46 : If the target is in low power mode, please enable "Debug in Low Power mode" option from Target->settings menu.

So probably something in your code explicitly disabling the debug interface, reconfiguring the the PA13/PA14 pins associated with the connection, or powering down the circuitry that connects.

Watch external clock vs HSE_VALUE definition, or setting clocks or PLL's beyond operating ranges.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
TDK
Super User

Does your program enter low power mode or repurpose the SWD pins? Either of those will produce this result.

If you feel a post has answered your question, please click "Accept as Solution".