Question
STM32F3 Discovery Running Code
Posted on June 18, 2013 at 20:47
This is a really basic question, but I'm just starting out on this board. I've been able to run programs through the Debug interface of ST-Link in Eclipse. Now I'm trying to get printf working with USART2, so I need the miniB cable attached to the breakout board I'm attaching to the board pins for Tx and Rx which means I can't really run through Debug mode because ST-Link needs the MiniB cable attached only to the ST-Link USB and not to the breakout board.
I was wondering how to run a program that is loaded onto flash memory without using Debug mode. I'm assuming there should be some easy way to run a program via one of the buttons or something, but i'm pretty clueless. The board is being powered through the breakout board I'm using. Thanks for the help in advance!