cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F207 DMA ADC Read with pin state change

joel239955_st
Associate
Posted on October 19, 2015 at 17:02

Hi, is it possible to have the pin state changed during ADC DMA Regular Simultaneous mode so that the pin that has been read is set to OUTPUT LOW while the one that is read is INPUT?

The current otherwise leaks through the other open analog PINs in my application and the PINs aren't independent anymore. 

I.e. I want to read 24 analog ports (or as many as possible) in sequence using DMA with only one open at a time. It currently works but I need to have all ports open.

Regards,

Joel Metelius
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on October 19, 2015 at 17:12

I don't think so.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Posted on October 19, 2015 at 22:19

> The current otherwise leaks through the other open analog PINs in my application and the PINs aren't independent anymore. 

Why do you think so?

What is the impedance of the signal source, and what is the settling time?

JW