cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F10x DSP library, where is it?

ioannis2
Associate II
Posted on May 17, 2013 at 09:48

I looking for a download link of the STM32F10x DSP Library, there multiple references to it and a user manual (UM0585) but cannot find the actual code anywhere... Anyone?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
frankmeyer9
Associate II
Posted on May 17, 2013 at 13:49

It is at least explicitely available for ST's M4 cores, say, the F3 and the F4, where you can download it as STM32Fxxx_DSP_StdPeriphLib_Vxxx.

The DSP part is provided by ARM, and can be used/compiled for M0, M3 and M3 cores.

Perhaps ST doesn't see DSP-like applications as a primary market for the F1xx series

ioannis2
Associate II
Posted on May 20, 2013 at 11:34

Well, I have inherited a project that uses the fore mentioned library but modified without explicit comments...The original lib is actually written by ST and is in assembly. I need to get my hands on the  original lib so I can do a diff to evaluate the modifications that have been performed... I suppose it must have been moved to the legacy staff, but nevertheless I need access to it.

Anybody?

zzdz2
Associate II
Posted on May 20, 2013 at 12:56

It looks like I never installed it but the installer itself is still on my drive, file attached.

________________

Attachments :

um0585.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0r7&d=%2Fa%2F0X0000000beW%2FlGmMORuX2BlUJRcE2BLkDhbyvetWUgfKAjYulaCMOn4&asPdf=false