cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F10x CanBus Recieve interrupt problem

ferhatyol-23
Senior
Posted on August 16, 2014 at 11:40

Hi there!

I'm using STM32F103VeT6 andI'm trying to do can bus communicationwith LoopBack Mode. This is my code.

/*******************************************************************************
* @file can.c
* @author Arectron
* @version V1.0.0
* @date 10/08/2014 
********************************************************************************/
/*-------------------------------Includes------------------------------------*/
#include ''STM32F10x.h''
#include ''CAN.h''
/* Private variables ---------------------------------------------------------*/
//CanRxMsg RxMessage;
/* Private Functions ---------------------------------------------------------*/
/*******************************************************************************
* Function Name : NVIC_Configuration
* Description : Configures the nested vectored interrupt controller.
* Input : None
* Output : None
* Return : None
* Attention : None
*******************************************************************************/
void NVIC_Configuration(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
#ifdef VECT_TAB_RAM 
/* Set the Vector Table base location at 0x20000000 */ 
NVIC_SetVectorTable(NVIC_VectTab_RAM, 0x0); 
#else /* VECT_TAB_FLASH */
/* Set the Vector Table base location at 0x08000000 */ 
NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x0); 
#endif
/* Enable CAN1 RX0 interrupt IRQ channel */
NVIC_InitStructure.NVIC_IRQChannel = USB_LP_CAN1_RX0_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
/*******************************************************************************
* Function Name : GPIO_Configuration
* Description : Configures the CAN GPIO ports.
* Input : None
* Output : None
* Return : None
* Attention : None
*******************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* CAN Periph clock enable */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO ,ENABLE);
/* Configure CAN pin: RX */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;
GPIO_Init(GPIOB, &GPIO_InitStructure); 
/* Configure CAN pin: TX */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_Init(GPIOB, &GPIO_InitStructure); 
GPIO_PinRemapConfig(GPIO_Remap1_CAN1,ENABLE);
}
/*******************************************************************************
* Function Name : CAN_init
* Description : Configures the CAN
* Input : None
* Output : None
* Return : None
* Attention : None
*******************************************************************************/
void Can_init(void)
{
CAN_InitTypeDef CAN_InitStructure;
CAN_FilterInitTypeDef CAN_FilterInitStructure;
RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE); 
NVIC_Configuration();
GPIO_Configuration();
CAN_DeInit(CAN1);
CAN_StructInit(&CAN_InitStructure);
/* CAN cell init */
CAN_InitStructure.CAN_TTCM=DISABLE;
CAN_InitStructure.CAN_ABOM=DISABLE;
CAN_InitStructure.CAN_AWUM=DISABLE;
CAN_InitStructure.CAN_NART=DISABLE;
CAN_InitStructure.CAN_RFLM=DISABLE;
CAN_InitStructure.CAN_TXFP=DISABLE;
CAN_InitStructure.CAN_Mode=CAN_Mode_LoopBack;
CAN_InitStructure.CAN_SJW=CAN_SJW_1tq;
CAN_InitStructure.CAN_BS1=CAN_BS1_8tq;
CAN_InitStructure.CAN_BS2=CAN_BS2_7tq;
CAN_InitStructure.CAN_Prescaler=1;
CAN_Init(CAN1,&CAN_InitStructure); 
/* CAN filter init */
CAN_FilterInitStructure.CAN_FilterNumber=0;
CAN_FilterInitStructure.CAN_FilterMode=CAN_FilterMode_IdMask;
CAN_FilterInitStructure.CAN_FilterScale=CAN_FilterScale_32bit;
CAN_FilterInitStructure.CAN_FilterIdHigh=0x0000;
CAN_FilterInitStructure.CAN_FilterIdLow=0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdHigh=0x0000;
CAN_FilterInitStructure.CAN_FilterMaskIdLow=0x0000;
CAN_FilterInitStructure.CAN_FilterFIFOAssignment=0;
CAN_FilterInitStructure.CAN_FilterActivation=ENABLE;
CAN_FilterInit(&CAN_FilterInitStructure);
CAN_ITConfig(CAN1,CAN_IT_FMP0, ENABLE);
}
/*******************************************************************************
* Function Name : CanSendMessage
* Description : Can Write Date to CAN-BUS
* Input : None
* Output : None
* Return : None
* Attention : None
*******************************************************************************/
ErrorStatus CanSendMessage(uint32_t CanTxId, uint8_t CanTxBufSize, uint8_t* CanTxData)
{
CanTxMsg TxMessage;
uint8_t i=0,CanTxMailbox=0,TimeOut=0;
/* transmit */
TxMessage.StdId = CanTxId; 
TxMessage.RTR = CAN_RTR_DATA;
TxMessage.IDE = CAN_ID_STD; 
TxMessage.DLC = CanTxBufSize; 
for(i=0;i<CanTxBufSize;i++)
{
TxMessage.Data[i]=CanTxData[i];
}
CanTxMailbox=CAN_Transmit(CAN1,&TxMessage);
TimeOut = 0;
// while((CAN_TransmitStatus(CAN1,CanTxMailbox) != CANTXOK))
// {
// TimeOut++;
// if(TimeOut==255)return ERROR;
// }
return SUCCESS;
}

The above program works without Recieve interrupts. So I can send and receive data.But when I interrupt active, the program doesn't work. This is interrupt rutine

void USB_LP_CAN_RX0_IRQHandler(void)
{
CanRxMsg RxMessage;
CAN_Receive(CAN1, CAN_FIFO0, &RxMessage);
lcd_set_cursor(0,1);
sprintf(dz,''ID=0x%X'',RxMessage.StdId);
lcd_print(dz);
CAN_ClearITPendingBit(CAN1,CAN_IT_FMP0);
}

What is the cause of the problem?

Regards

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0