cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F107VC CAN bus pin remap

hello
Associate II
Posted on June 20, 2012 at 23:19

hi.

i am using the STM32F107VC board from IAR i have some example code for CAN but in my Board they used the PD0 and PD1 for CAN i dont know how to remap it in my code. i have 2 board and i want to sent data between 2 boards.

void GPIO_Configuration(void)

{

  GPIO_InitTypeDef  GPIO_InitStructure;

  

 // GPIO_PinRemapConfig(GPIO_Remap2_CAN1 , ENABLE);

  /* Configure CAN pin: RX */

  //GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_CAN_RX;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;

  GPIO_Init(GPIO_CAN, &GPIO_InitStructure);

  

  /* Configure CAN pin: TX */

  //GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_CAN_TX;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_Init(GPIO_CAN, &GPIO_InitStructure);

  

  GPIO_PinRemapConfig(GPIO_Remap_CAN , ENABLE);

}

can any one pls help me solve this problem..

thanks...

This discussion is locked. Please start a new topic to ask your question.
20 REPLIES 20
Posted on June 21, 2012 at 00:50

Probably not enabling the AFIO clock.

/* Enable GPIOD and AFIO clocks for remapping */
RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOD, ENABLE);
/* Configure CAN1 RX pin */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU;
GPIO_Init(GPIOD, &GPIO_InitStructure);
/* Configure CAN1 TX pin */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOD, &GPIO_InitStructure);
/* Remap CAN1 GPIOs */
GPIO_PinRemapConfig(GPIO_Remap2_CAN1 , ENABLE); /* PD 0 and 1 */
/* CAN1 Periph clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE);
/* CAN1 register init */
CAN_DeInit(CAN1);
// ...

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
hello
Associate II
Posted on June 21, 2012 at 01:15

i change accordingly but It also not working....

readme.txt say's like

Connectivity line devices are STM32F105xx and STM32F107xx microcontrollers.

STM3210C-EVAL (STM32F10x -- Connectivity line)

my LED r connected in my board to PC.06, PC.07, PC.08 and PC.09 pins

which suits with set-up 

- STM3210B-EVAL Set-up  

    - Use LED1, LED2, LED3 and LED4 leds connected respectively to PC.06, PC.07, PC.08

      and PC.09 pins

    - Use Push Button connected to PB9      

    - Connect a female/female CAN cable between at least 2 EVAL CAN connectors 

      (on STM3210B-EVAL (CN2)/ STM3210E-EVAL (CN4) boards) 

      - Connector 1 DB9_PIN2 to Connector 2 DB9_PIN2  (CAN_L)

  - Connector 1 DB9_PIN5 to Connector 2 DB9_PIN5  ( GND )

  - Connector 1 DB9_PIN7 to Connector 2 DB9_PIN7  (CAN_H) 

  @note JP3 must be fitted.

  

@note Any unit in the CAN bus may play the role of sender (by pressing on the 

      key) or receiver.

so because of LED i am using STM3210B-EVAL Set-up 

 

how can i change the LED pin if i use 

STM3210C-EVAL Set-up 

    - Use LED1, LED2, LED3 and LED4 connected respectively to PD.07, PD.13, PF.03

      and PD.04 pins

    - Use Push Button connected to PB9

    - Connect a female/female CAN cable between at least 2 EVAL CAN connectors 

      (on STM3210E-EVAL (CN2)/ STM3210C-EVAL (CN3) boards)

       - Connector 1 DB9_PIN2 to Connector 2 DB9_PIN2  (CAN_L)

   - Connector 1 DB9_PIN5 to Connector 2 DB9_PIN5  ( GND )

   - Connector 1 DB9_PIN7 to Connector 2 DB9_PIN7  (CAN_H) 

  @note JP6 or JP5 must be fitted.

as in my board LED r connected to PC.06, PC.07, PC.08 and PC.09 pins

thanks...

Posted on June 21, 2012 at 02:35

Ok, so what board do you actually have? Does it have a revision number?

The STM3210C-EVAL, from ST, has CN3 connected to PD0,1 for CAN1 and LD1/LED1 is PD7

Get a schematic for your IAR board and determine what is connected where.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
hello
Associate II
Posted on June 21, 2012 at 03:12

thanks for your reply..

i use

IAR KickStart Kit for STM32F107VC

i have attached theschematic of my board in this.

in my board the pin are

LED1(STAT1)- PC6

LED2(STAT2)- PC7

LED3(STAT3)- PC8

LED4(STAT4)- PC9

CAN1_TX - PD1

CAN1_RX - PD0

CAN1_CNTRL - PD14

there is Jumper settings in my board:

CAN1_T

OPEN- CAN1 Termination Disable

CLOSE- CAN1 Termination Enable(Default)

i have not change any of jumper its CLOSE i guess...

thanks...

________________

Attachments :

IAR-STM32F107VC-SK_REV-1.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0fw&d=%2Fa%2F0X0000000bea%2FmJ66jtfM39hbTgLWLlmyEJ8r_R87kfybaO3TzS1ZflU&asPdf=false
Posted on June 21, 2012 at 04:37

Then you'll need to configure PD14 as a GPIO output, and drive it appropriately to enable the transceiver. The ST boards have a jumper to VCC or GND

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
hello
Associate II
Posted on June 21, 2012 at 11:24

can you please expline me shortly about GPIO config PD14...

Posted on June 21, 2012 at 23:15

can you please expline me shortly about GPIO config PD..

Really? If I scan the schematic and datasheet correctly :

/* Configure PD14 in output pushpull mode */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_14;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
GPIO_Init(GPIOD, &GPIO_InitStructure);
Then
GPIO_SetBits(GPIOD, GPIO_Pin_14); // Set Transceiver in Transmit Enable (Dominant when CAN_TX LOW, otherwise Recessive)

or
GPIO_ResetBits(GPIOD, GPIO_Pin_14); // Set Transceiver in Receive Only

http://www.ti.com/lit/ds/symlink/sn65hvdpdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
hello
Associate II
Posted on June 22, 2012 at 00:51

Hi,

thanks for your reply and for your time

i did so still no change...i am trying it for long time but noting happening...

Posted on June 22, 2012 at 01:05

Time to break out the oscilloscope.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..