STM32F105 USART2's DR register not working
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-07-18 4:48 AM
Hi all,
I'm trying to use the USART2 on the STM32F105CL to communicate with an hyper-terminal but unfortunatly, the hyper-terminal is not receiving anything. Even with a very simple code./* Includes ------------------------------------------------------------------*/#include <stdio.h>#include <string.h>#include ''stm32f10x.h''#include ''stm32f10x_gpio.h''#include ''stm32f10x_rcc.h''#include ''stm32f10x_usart.h''#include ''leds.h''/* Private typedef -----------------------------------------------------------*//* Private define ------------------------------------------------------------*//* Private macro -------------------------------------------------------------*//* Private variables ---------------------------------------------------------*//* Private function prototypes -----------------------------------------------*//* Private functions ---------------------------------------------------------*/int main(void){ LED_Init(); /* ************************************************************/ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; /* Enable GPIO clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_AFIO, ENABLE); /* Enable USART clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); GPIO_PinRemapConfig(GPIO_Remap_USART2, ENABLE); //Configure USART2 pins: Rx and Tx ---------------------------- GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_Init(GPIOA, &GPIO_InitStructure); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 57600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2,ENABLE); /* ********************************************/ while (1) { for(int i=0;i<100000;i++) { LED_On(); } for(int i=0;i<100000;i++) { LED_Off(); } while(USART_GetFlagStatus(USART2,USART_FLAG_TC) == RESET){}; USART_SendData(USART2,'a'); while(USART_GetFlagStatus(USART2,USART_FLAG_TXE) == RESET){}; } return 0;}Sombody has any clue ?Thanks,- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-07-18 8:05 AM
So,
Tool chain : gccLibrary's version : V3.5.0- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-07-18 8:08 AM
Sorry, the RESET Value is 0
''typedef enum {RESET = 0, SET = !RESET} FlagStatus, ITStatus;''- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-07-18 8:23 AM
Why are you remapping the pins? PA2/3 are the default exit points for USART2, PD5/6 are the remapped ones.
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-07-18 8:41 AM
Which version of GNU/GCC? Who's package? As you mentioned HyperTerminal, assuming a Windows platform.
Attached is a USART2 demo, I would have added LEDs but neither your board, or configuration has been expressed. The .HEX should output a stream of 'a' characters at 57600 8N1 ________________ Attachments : USART2-CL.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0qo&d=%2Fa%2F0X0000000bef%2F0GcopP7AvKDV8hLcealkR17XvyVyR_xtY9ODL6qQEVk&asPdf=falseUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-07-20 11:52 PM
YOU... ARE..... SO.. GENIOUS !!!
The problem was the remapping. I comment the line and it works (once...).After one success, i've got a infinite loop when I wait for the TXE flag to be SET.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-07-21 12:54 AM
Funny, the problem seems to be the STlink V2.
When I put the power on the STM32f105, so he runs the last code flashed on it, it works...When I pass through the Eclipses debugger, I have the infinite loop.Don't know why but w/e.
- « Previous
-
- 1
- 2
- Next »