Question
STM32F105 Shared Pin PA9 (USART1-TX and VBUS) conflict
Posted on January 05, 2014 at 19:36
Hello,
the STM32F105 Device share USART1-TX and VBUS for USB on Port PA9. I need the USART1 for communication and for the internal Bootloader (only USART1 on my used 64pin Devices possible), if the firmware corrupts. I need the USB-Device possibility for connecting the Device to a HOST-PC sometimes, but its not used for the internal Bootloader. The other STM Devices with only USB-Device function don�t have a VBUS port und use an external resistor for USB recognition. My question is: Can I switch off the VBUS - Port on PA9, still use the STM32F105 as a USB-Device (with external USB Resistor), and use the PA9 for the USART1-TX? Thank you Rheinhold #stm32f105-pa9-usart1-vbus