cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f105 HOST USB

sami
Associate II
Posted on January 10, 2012 at 17:12

Hello

I am designing a new project with stm32f105 ; i need a host usb ; i have checked the development kits i found they use usb_id; but i need to use A-type connector ; so if if i leave usb_id floating ; is there any problem since i will use the usb_library from st ?

Regards

Sami
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
rosarium
Associate II
Posted on January 11, 2012 at 06:02

Can you explain a bit more. Which id you are talking about?

And also lemme know which application you want to develop Host_MSC or Host_HID??