2010-07-23 9:22 AM
STM32F105 DFU - how much current does it draw on PA9 pin?
2011-08-08 3:01 PM
The following measurements were made with a series resistor between USB_VBUS and PA9. The results imply that there is an equivalent of a 26.5K internal pull-down on PA9/OTG_FS_VBUS. Perhaps an internal voltage divider for comparator and detection of OTG_FS_VBUS?
USB_VBUS ---/\/\/\/\------ PA9
5V 6.4K 4V
USB_VBUS ---/\/\/\/\------ PA9
5V 2.644K 4.5V